Join our 30-minute expert session on July 10, 2025 (9:00 AM & 5:00 PM CET), to explore Digital Twins, cooling simulations, and IT infrastructure modeling. Learn how to boost resiliency and plan power capacity effectively. Register now to secure your spot!

BACnet blacklist implementation to disable features in an EBO Server BACnet interface.

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • BACnet blacklist implementation to disable features in an EBO Server BACnet interface.
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • RobertAndriolo
    RobertAndriolo
  • RandyDavis
    RandyDavis
  • David_Purser
    David_Purser
  • GavinHe
    GavinHe
  • David_Kendrick
    David_Kendrick
  • DavidChild
    DavidChild
  • CraigEl
    CraigEl
  • PaulFr
    PaulFr
  • Kim_Baze
    Kim_Baze
  • Benji
    Benji
  • AbeMeran
    AbeMeran
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
3 Likes
7218 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

BACnet blacklist implementation to disable features in an EBO Server BACnet interface.

Picard Product_Support
‎2018-09-12 12:19 AM

Last Updated: Administrator CraigEl Administrator ‎2024-10-30 05:33 PM

Issue

Some BACnet devices advertise support for services such as RPM, COV, etc but malfunction when the service is used. An example of such a device is the Johnson Controls TEC2627VVT which advertises support for RPM but fails to upload its objects when SBO uses RPM to get the object list.

Product Line

EcoStruxure Building Operation

Environment

  • BACnet
  • Automation Server
  • Enterprise Server

Cause

Some BACnet devices with inconsistent protocol implementation cannot process BACnet services such as RPM, COV, etc.

Resolution

Feature Supported in Version
<no-rpm/> 1.8.1 and higher
<no-cov/> 1.8.1.23701 and higher
<ignore-unhosted-devices/> 3.2.3.9005 and higher (*)

 

Users can create a rule under the BACnet interface to configure SBO not to use the service. Some rules are global, while others can be for specific BACnet devices. For particular BACnet devices, they are specified by 'Vendor Identifier' and 'Model Name,' which need to match exactly as shown in that device's Properties - Advanced Tab.

 

  1. Ensure you have installed the version that supports the feature you want to change.
  2. Setup file using the no-rpm rule.
    1. Use a text editor like 'Notepad' to create a text file or download the same file below.
    2. Enter the device's vendor ID (5)  and model name (TEC2627VVT) followed by the rule (no-rpm) using the format seen in the screenshot below.
    3. Save the file to the desired location on the PC with a name aiding later identification.rpm.png
    4. Under the BACnet interface, create a new 'Document' object in the 'Application' folder.
    5. NOTE: The object MUST be named 'service_blacklist' in all lowercase.
    6. Click 'Next,' import the text file created in step 1, and save the 'Document' object.
    7. Restart the Server NoRPM_WarmStart_new.PNG
    8. Once the device is on the block list, SBO will not send 'readPropertyMultiple' requests to the device using only individual 'readProperty' requests. Add the service_blacklist to the EBO Server.
  3. Add the no-cov tag if you would like to block that service for this device:  rpm and cov.png
  4. Extended for multiple devices from different vendors simultaneously using this example for reference.   multiple.png
  5. One can add a global rule using this syntax to ignore unhosted devices.
    1. * NOTE: It is recommended to remove <ignore-unhosted-devices/> after upgrading to EBO 4.0/2022 and higher because this feature is supported in the BACnet Interface Properties and BACnet Device Discovery view. Device Discovery for BACnet Controllers and IO Modules (se.com) IgnoreUnhostedDevices.png
  6. Once the Server has restarted, check the trace.log file and search for service_blacklist, there should be entries similar to this.  Tracelog Blacklist Message.png
Labels (1)
Labels:
  • EcoStruxure Building Operation
Attachments
Tags (4)
  • Find more articles tagged with:
  • 19120
  • DavidPurser23
  • GavinHeward23
  • qc33462
Was this article helpful? Yes No
100% helpful (11/11)

Link copied. Please paste this link to share this article on your social media post.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.