Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Schneider Electric Community
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
  • About Mumuny_Gbadamosi
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Mumuny_Gbadamosi
Mumuny_Gbadamosi
Explorer
‎2026-09-04
29
Posts
16
Likes Received
0
Likes Given
0
Solutions

Community Badges

Resistance is Futile - L4
Live Long and Prosper - L3
Resistance is Futile - L3
Live Long and Prosper - L2
+6
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
Mumuny_Gbadamosi
Mumuny_Gbadamosi Explorer

How to integrate Modicon Edge IO NTS in M580 systems using the built-i...

IssueTo configure and establish an EtherNet/IP communication between an M580 controller and an Edge I/O NTS island, the I/O system's EDS file needs to...
Knowledge Center icon_circle Industrial Automation Knowledge Base
14128 2 0

2025-05-22 02:51 PM

Mumuny_Gbadamosi
Mumuny_Gbadamosi Explorer

How to integrate Modicon Edge IO NTS in M580 systems using the built-i...

IssueIn Control Expert, a generic modbus DTM can be configured to establish a modbus communication between an M580 controller and an Edge I/O NTS isla...
Knowledge Center icon_circle Industrial Automation Knowledge Base
11205 1 0

2025-05-22 02:23 PM

Mumuny_Gbadamosi
Mumuny_Gbadamosi Explorer

Modicon M580 Redundant I/O Network - High-Availability Architecture Co...

IssueHow to configure and implement redundant I/O network using PRP technology within a Modicon M580 High-Availability Architecture? ResolutionThis a...
Knowledge Center icon_circle Industrial Automation Knowledge Base
13368 2 0

2025-03-25 01:10 PM

Mumuny_Gbadamosi
Mumuny_Gbadamosi Explorer

Modicon M580 Redundant I/O Network - Standalone Architecture Configura...

IssueHow to configure and implement redundant I/O network using PRP technology within a Modicon M580 standalone architecture? ResolutionThis article ...
Knowledge Center icon_circle Industrial Automation Knowledge Base
9653 1 0

2025-03-11 05:41 AM

Mumuny_Gbadamosi
Mumuny_Gbadamosi Explorer

Modicon Edge I/O NTS - How to perform Bulk Firmware Update

IssueOnce a Modicon Edge I/O NTS distributed system is configured using the configurator or the web interface, the next step is to download the config...
Knowledge Center icon_circle Industrial Automation Knowledge Base
7609 0 0

2025-02-12 10:51 AM

Mumuny_Gbadamosi
Mumuny_Gbadamosi Explorer

Modicon M580 - Communication with Modicon Edge I/O NTS

IssueI need to establish communication between an M580 controller and a Modicon Edge I/O NTS distributed system.ResolutionThis article provides a step...
Knowledge Center icon_circle Industrial Automation Knowledge Base
9910 4 0

2025-02-11 04:50 AM

Mumuny_Gbadamosi
Mumuny_Gbadamosi Explorer

Modicon Edge I/O NTS - NTSNEC1200 Firmware Upgrade

IssueI would like to upgrade the firmware of my Modicon Edge I/O NTS Network Interface Module to overcome published vulnerabilities identified in the ...
Knowledge Center icon_circle Industrial Automation Knowledge Base
3807 2 0

2025-02-05 03:00 PM

Mumuny_Gbadamosi
Mumuny_Gbadamosi Explorer

Modicon Edge Compute Node - Backing Up Portainer Configuration

IssueHow to back up a portainer server configuration?ResolutionThis article describes the different steps to go through in order to create a backup of...
Knowledge Center icon_circle Industrial Automation Knowledge Base
2396 1 0

2024-12-30 10:26 AM

Mumuny_Gbadamosi
Mumuny_Gbadamosi Explorer

Modicon Edge Compute Node - Using Portainer Reset Password Helper

IssueWhat to do in case you've forgotten the password of the only administrator account of a portainer instance running inside the Modicon Edge Comput...
Knowledge Center icon_circle Industrial Automation Knowledge Base
4568 0 0

2024-12-28 08:55 AM

Mumuny_Gbadamosi
Mumuny_Gbadamosi Explorer

Modicon Edge Compute Node - Implementing Node-Red in M580 systems

IssueI would like to implement Node-Red in an existing M580 system without the need to install a dedicated iPC hardware .ResolutionThis article provid...
Knowledge Center icon_circle Industrial Automation Knowledge Base
4849 1 0

2024-12-27 01:57 AM

Mumuny_Gbadamosi
Mumuny_Gbadamosi Explorer

Modicon Managed Switch - Firmware Update using the Web Interface

IssueI would like to upgrade the firmware of my Modicon Switch to overcome published vulnerabilities identified in the previous firmware version or ga...
Knowledge Center icon_circle Industrial Automation Knowledge Base
2822 0 0

2024-06-30 06:40 PM

Activity Feed
  • Got a Like for Modicon M580 - Communication with Modicon Edge I/O NTS. ‎2026-07-10 03:28 AM
  • Got a Like for How to Clear the EcoStruxure Control Expert Security Editor Tools Database. ‎2026-04-08 03:02 PM
  • Got a Like for Modicon Edge Compute Node - Backing Up Portainer Configuration. ‎2026-02-19 11:36 PM
  • Got a Like for Modicon Edge I/O NTS - NTSNEC1200 Firmware Upgrade. ‎2025-08-18 04:53 AM
  • Got a Like for How to integrate Modicon Edge IO NTS in M580 systems using the built-in EtherNet/IP DTM. ‎2025-07-15 12:49 PM
  • Got a Like for Modicon M580 Redundant I/O Network - High-Availability Architecture Configuration. ‎2025-05-24 04:02 AM
  • Got a Like for How to integrate Modicon Edge IO NTS in M580 systems using the built-in EtherNet/IP DTM. ‎2025-05-24 04:00 AM
  • Got a Like for How to integrate Modicon Edge IO NTS in M580 systems using the built-in Modbus DTM. ‎2025-05-24 04:00 AM
  • Posted How to integrate Modicon Edge IO NTS in M580 systems using the built-in EtherNet/IP DTM on Industrial Automation Knowledge Base. ‎2025-05-22 02:51 PM
  • Posted How to integrate Modicon Edge IO NTS in M580 systems using the built-in Modbus DTM on Industrial Automation Knowledge Base. ‎2025-05-22 02:23 PM
  • Got a Like for Modicon M580 Redundant I/O Network - High-Availability Architecture Configuration. ‎2025-03-26 01:43 AM
  • Posted Modicon M580 Redundant I/O Network - High-Availability Architecture Configuration on Industrial Automation Knowledge Base. ‎2025-03-25 01:10 PM
  • Got a Like for Modicon M580 Redundant I/O Network - Standalone Architecture Configuration. ‎2025-03-13 09:53 AM
  • Posted Modicon M580 Redundant I/O Network - Standalone Architecture Configuration on Industrial Automation Knowledge Base. ‎2025-03-11 05:41 AM
  • Got a Like for Modicon M580 - Communication with Modicon Edge I/O NTS. ‎2025-03-10 03:16 PM
  • Got a Like for Modicon M580 - Communication with Modicon Edge I/O NTS. ‎2025-02-20 01:22 AM
  • Posted Modicon Edge I/O NTS - How to perform Bulk Firmware Update on Industrial Automation Knowledge Base. ‎2025-02-12 10:51 AM
  • Got a Like for Modicon Edge I/O NTS - NTSNEC1200 Firmware Upgrade. ‎2025-02-12 08:21 AM
  • Got a Like for Modicon M580 - Communication with Modicon Edge I/O NTS. ‎2025-02-12 08:21 AM
  • Posted Modicon M580 - Communication with Modicon Edge I/O NTS on Industrial Automation Knowledge Base. ‎2025-02-11 04:50 AM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.