• About Sepehr_Zarrabi
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Sepehr_Zarrabi
Sepehr_Zarrabi
Lieutenant
‎2025-11-04
87
Posts
12
Likes Received
7
Likes Given
6
Solutions

Community Badges

Open Hailing Frequencies - L5
Open Hailing Frequencies - L4
Resistance is Futile - L4
Live Long and Prosper - L3
+14
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
Sepehr_Zarrabi
/html/rank_icons/Lieutenant.png Sepehr_Zarrabi /html/rank_icons/SE-Employee.png

What is the accuracy of PM8000 for demand readings?

Looking for the accuracy of the following demand measurements in the PM8000: - Current demand - Active power demand - Reactive power demand - Apparent...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1715 0 3

2020-12-17 01:14 PM

Sepehr_Zarrabi
/html/rank_icons/Lieutenant.png Sepehr_Zarrabi /html/rank_icons/SE-Employee.png

ION8650 High Speed Data Recording

I have an application where we need to record Freq. and kW at 32 samples per second (not cycles). A Setpoint module will trigger the recording if the...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2311 0 3

2020-04-02 03:45 PM

Sepehr_Zarrabi
/html/rank_icons/Lieutenant.png Sepehr_Zarrabi /html/rank_icons/SE-Employee.png

PT's Appropriate for fast transient detection in ION9000T

Given the high sampling rate of the ION9000T, what Potential Transformers (PT's) do you recommend for monitoring a 15kV system? The concern is that a ...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1196 0 1

2020-03-09 04:48 PM

Sepehr_Zarrabi
/html/rank_icons/Lieutenant.png Sepehr_Zarrabi /html/rank_icons/SE-Employee.png

Calculate Standard Deviation in an ION Meter

Is it possible to somehow calculate Standard Deviation in an ION meter (ideally PM8000)? We have an opportunity to sell multiple PM8000's to a firm th...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2363 0 4

2019-07-17 02:34 PM

Sepehr_Zarrabi
/html/rank_icons/Lieutenant.png Sepehr_Zarrabi /html/rank_icons/SE-Employee.png

PM5000 & PM8000 Demand Register Scaling

In case of PM5563 and also PM8000 does the demand shown on the meter display switch between kW, MW, GW ? If so, what is the boundary at which this swi...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2056 0 2

2019-03-19 08:45 AM

Sepehr_Zarrabi
/html/rank_icons/Lieutenant.png Sepehr_Zarrabi /html/rank_icons/SE-Employee.png

Trigger 128 point/cycle waveform captures on CM2

The CM2xxx meter can capture 64 and 128 point/cycle waveforms. In SMS and PMCU software, the user can manually trigger both the high-resolution and th...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2387 0 7

2018-07-26 02:19 PM

Sepehr_Zarrabi
/html/rank_icons/Lieutenant.png Sepehr_Zarrabi /html/rank_icons/SE-Employee.png

ION6200 Factory Reset

Is it possible to factory reset an ION6200 meter in the field? I know about the "Reset Mode" that resets energy, demand, etc. but I need to reset all ...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2264 0 5

2018-05-15 04:47 PM

Sepehr_Zarrabi
/html/rank_icons/Lieutenant.png Sepehr_Zarrabi /html/rank_icons/SE-Employee.png

Is the dual Ethernet ports in the new PM meters a true Ethernet switch...

Can the dual Ethernet ports in the back of the PM5000 or PM8000 be used as an Ethernet switch to transport other protocols? For example let's say ther...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1328 0 2

2016-11-02 02:02 PM

Sepehr_Zarrabi
/html/rank_icons/Lieutenant.png Sepehr_Zarrabi /html/rank_icons/SE-Employee.png

ION7550 / 7650 Ethernet Card Firmware Requirements

A customer has some relatively old ION7500, ION7600, ION7550, ION7650 meters. I think the oldest one is an ION7500 with firmware rev 7500V207. They wa...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
817 0 1

2016-10-03 05:33 PM

Sepehr_Zarrabi
/html/rank_icons/Lieutenant.png Sepehr_Zarrabi /html/rank_icons/SE-Employee.png

ION Enterprise 6.0 & BCPM

1) Is it possible to use ION Setup to configure the Veris BCPM such that it groups 2-pole and 3-pole breakers?2) Would the device driver in ION Enterp...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
735 0 0

2016-03-08 04:05 PM

Sepehr_Zarrabi
/html/rank_icons/Lieutenant.png Sepehr_Zarrabi /html/rank_icons/SE-Employee.png

Can the ION7650 Hardware Lock Be Removed in the Field?

Customer has ordered an ION7650 with hardware lock. Apparently it was a mistake and they do not want it to be locked. Can this be changed in the field...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1003 0 1

2016-01-14 10:25 AM

Activity Feed
  • Posted Re: Error message while configuring email alerts in PME 2021 having ENM license on Power Monitoring and Energy Automation NAM. ‎2022-10-10 08:51 AM
  • Tagged Re: Error message while configuring email alerts in PME 2021 having ENM license on Power Monitoring and Energy Automation NAM. ‎2022-10-10 08:51 AM
  • Liked Get this new approach to evaluating Voltage Sags for Sreemant_Roy. ‎2022-09-23 11:54 AM
  • Posted Re: Get this new approach to evaluating Voltage Sags on Metering & Power Quality. ‎2022-09-23 11:26 AM
  • Tagged Re: Get this new approach to evaluating Voltage Sags on Metering & Power Quality. ‎2022-09-23 11:26 AM
  • Posted Re: What is the accuracy of PM8000 for demand readings? on Metering & Power Quality. ‎2021-01-04 08:26 AM
  • Tagged Re: What is the accuracy of PM8000 for demand readings? on Metering & Power Quality. ‎2021-01-04 08:26 AM
  • Posted What is the accuracy of PM8000 for demand readings? on Metering & Power Quality. ‎2020-12-17 01:14 PM
  • Tagged What is the accuracy of PM8000 for demand readings? on Metering & Power Quality. ‎2020-12-17 01:14 PM
  • Got a Like for Re: ION8650 High Speed Data Recording. ‎2020-04-09 11:33 AM
  • Posted Re: ION8650 High Speed Data Recording on Metering & Power Quality. ‎2020-04-08 09:01 AM
  • Posted ION8650 High Speed Data Recording on Metering & Power Quality. ‎2020-04-02 03:45 PM
  • Tagged ION8650 High Speed Data Recording on Metering & Power Quality. ‎2020-04-02 03:45 PM
  • Posted PT's Appropriate for fast transient detection in ION9000T on Metering & Power Quality. ‎2020-03-09 04:48 PM
  • Tagged PT's Appropriate for fast transient detection in ION9000T on Metering & Power Quality. ‎2020-03-09 04:48 PM
  • Posted Re: Calculate Standard Deviation in an ION Meter on Metering & Power Quality. ‎2019-07-18 11:20 AM
  • Posted Calculate Standard Deviation in an ION Meter on Metering & Power Quality. ‎2019-07-17 02:34 PM
  • Posted Re: PM5000 & PM8000 Demand Register Scaling on Metering & Power Quality. ‎2019-03-27 08:41 AM
  • Posted PM5000 & PM8000 Demand Register Scaling on Metering & Power Quality. ‎2019-03-19 08:45 AM
  • Posted Re: Trigger 128 point/cycle waveform captures on CM2 on Metering & Power Quality. ‎2018-07-30 02:45 PM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.