Is the dual Ethernet ports in the new PM meters a true Ethernet switch (protocol agnostic)?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Is the dual Ethernet ports in the new PM meters a true Ethernet switch (protocol agnostic)?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Picard Charles_Murison Picard
525
Mehran_Mehrnia
Admiral Mehran_Mehrnia Admiral
138
Ramasamy_N
Captain Ramasamy_N Captain
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Sepehr_Zarrabi
Lieutenant Sepehr_Zarrabi Lieutenant
Lieutenant

Posted: ‎2016-11-02 02:02 PM

0 Likes
2
1363
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
‎2016-11-02 02:02 PM

Is the dual Ethernet ports in the new PM meters a true Ethernet switch (protocol agnostic)?

Can the dual Ethernet ports in the back of the PM5000 or PM8000 be used as an Ethernet switch to transport other protocols? For example let's say there is a PM8000 and downstream from it is a BACnet device. Can we use one of the ports on the PM8000 to communicate ION to the meter itself and use the second port to have the BMS system communicate to the downstream device via BACnet?

Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Anonymous user
Not applicable

Posted: ‎2016-11-10 09:48 AM

0 Likes
0
1294
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
‎2016-11-10 09:48 AM

Sepehr,

The two (2) Ethernet ports on the PM5000 and PM8000 function as an Ethernet switch and are completely protocol agnostic.  You could connect a PC on the second port or other TCP/IP client or server and it would see no difference in network accessiblity.

Regards,

James Clark

See Answer In Context

Reply
Replies 2
Sepehr_Zarrabi
Lieutenant Sepehr_Zarrabi Lieutenant
Lieutenant

Posted: ‎2016-11-10 09:02 AM

0 Likes
0
1294
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
‎2016-11-10 09:02 AM

I would appreciate if someone could shed light on this question. Hal Etheridge, John Straughn

Thank you !

Reply
Anonymous user
Not applicable

Posted: ‎2016-11-10 09:48 AM

0 Likes
0
1295
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
‎2016-11-10 09:48 AM

Sepehr,

The two (2) Ethernet ports on the PM5000 and PM8000 function as an Ethernet switch and are completely protocol agnostic.  You could connect a PC on the second port or other TCP/IP client or server and it would see no difference in network accessiblity.

Regards,

James Clark
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.