Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Which Meters support a 200Vac and frequency of 400Hz ?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Which Meters support a 200Vac and frequency of 400Hz ?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
sesa213753
sesa213753 Leader
Leader

Posted: ‎2016-10-06 08:18 AM

0 Likes
4
1892
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
‎2016-10-06 08:18 AM

Which Meters support a 200Vac and frequency of 400Hz ?

Hi, of this families... may someone confirm me, if they support or no 200Vac/400Hz ?

PM1000

PM700

PM800

PM5000

PM8000

ION7400

ION7650

ION8650

best regards

James Jeanette

Tags (4)
  • Tags:
  • pm 8000
  • pm5000
  • pm700
  • pm800
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
DanL
DanL Champion
Champion

Posted: ‎2016-11-14 01:37 PM

0 Likes
0
1816
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
‎2016-11-14 01:37 PM

Just to clarify - Neither the PM8000 nor the ION7400 are rated to be powered at 200VAC 400Hz (120VAC is max for safety ratings at 400Hz).

However, both models can measure 200VAC at 400Hz. Most power quality parameters will not function above 70Hz (harmonics, flicker, etc). I believe all the ION meters also have these restrictions & limitations.

Gregory Lado  - I'm curious what is the application?

Thanks

Dan

See Answer In Context

Reply
Replies 4
Anonymous user
Not applicable

Posted: ‎2016-11-11 09:14 AM

0 Likes
0
1815
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
‎2016-11-11 09:14 AM

no one answered this and it's a shame since I have the same question today.

Reply
Sanjeet_Sahota
Sanjeet_Sahota Mentor
Mentor

Posted: ‎2016-11-14 09:00 AM

0 Likes
1
1815
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
‎2016-11-14 09:00 AM

Hi Jorge, and Gregory,


My apologies for not seeing this earlier. Digging a bit into this, it appears that I can confidently say the PM8000 and the ION7400 support the range specified.  However, the accuracy spec is not defined for this the 400Hz frequency, unfortunately. The accuracy spec is only defined for 42 Hz to 69 Hz range.


Best Regards,


Sanjeet

Reply
DanL
DanL Champion
Champion

Posted: ‎2016-11-14 01:37 PM

0 Likes
0
1816
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
‎2016-11-14 01:37 PM

Just to clarify - Neither the PM8000 nor the ION7400 are rated to be powered at 200VAC 400Hz (120VAC is max for safety ratings at 400Hz).

However, both models can measure 200VAC at 400Hz. Most power quality parameters will not function above 70Hz (harmonics, flicker, etc). I believe all the ION meters also have these restrictions & limitations.

Gregory Lado  - I'm curious what is the application?

Thanks

Dan

Reply
Anonymous user
Not applicable

Posted: ‎2016-11-14 02:11 PM

0 Likes
0
1815
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
‎2016-11-14 02:11 PM

From the users manual, PM800, CM2000, CM3000, CM4000 can monitor  400Hz power system, which could be seen in military application
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.