Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION8650 High Speed Data Recording

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • ION8650 High Speed Data Recording
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Sepehr_Zarrabi
Sepehr_Zarrabi Troubleshooter
Troubleshooter

Posted: ‎2020-04-02 03:45 PM

0 Likes
3
2649
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
‎2020-04-02 03:45 PM

ION8650 High Speed Data Recording

I have an application where we need to record Freq. and kW at 32 samples per second (not cycles). 

 

A Setpoint module will trigger the recording if the Frequency goes out of bounds. However, I cannot figure out if we can have a Data Recorder module log that fast. In the manual I see "HIGH SPEED CONTINUOUS" but I have not been able to figure out what that means.

 

1) Is it possible to record values at 32 samples per second.

2) The next part of the requirement is to also record an analog signal at the same rate (32 samples per second). Is the Analog Input module a high-speed module?

 

Thank you!

Tags (1)
  • Tags:
  • ion8650
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2020-04-02 04:48 PM

0 Likes
2
2645
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
‎2020-04-02 04:48 PM

Hello Sepehr,

 

1) Yes the meter is able to record values at a rate of 32 per second (period of 0.03125 seconds). I did test this on a meter with periodic timer of 0.031. The meter is able to record this fast. Note that this was also setup with the enable being controlled as to not have meter need to worry about wearing out the lash memory. 

 

Second part is to log the freq and kW, the default module for this is the power meter module, however this is updated only once a second. The high speed module does update at high speed. There is a catch however when using this module for frequency. The frequency measurement at this rate is susceptible to hysteresis and you may see a jump/dip in the value. The 1 second update is great without any issue and meets all standards we say the meter meets. However the HS power meter module has no standards for 1/2 cycle updates.

 

Second question: "record an analog signal at the same rate " I am afraid I do not have a meter with the IO module that I can test the update rate with. 

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 3
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2020-04-02 04:48 PM

0 Likes
2
2646
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
‎2020-04-02 04:48 PM

Hello Sepehr,

 

1) Yes the meter is able to record values at a rate of 32 per second (period of 0.03125 seconds). I did test this on a meter with periodic timer of 0.031. The meter is able to record this fast. Note that this was also setup with the enable being controlled as to not have meter need to worry about wearing out the lash memory. 

 

Second part is to log the freq and kW, the default module for this is the power meter module, however this is updated only once a second. The high speed module does update at high speed. There is a catch however when using this module for frequency. The frequency measurement at this rate is susceptible to hysteresis and you may see a jump/dip in the value. The 1 second update is great without any issue and meets all standards we say the meter meets. However the HS power meter module has no standards for 1/2 cycle updates.

 

Second question: "record an analog signal at the same rate " I am afraid I do not have a meter with the IO module that I can test the update rate with. 

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2020-04-02 04:55 PM

1 Like
0
2643
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
‎2020-04-02 04:55 PM

Small correction, I was looking at wrong document, I do not see analog inputs for the ION8650. I do see digital but that is not what I believe you are looking for.

 

Charles

 

L4 Prime for Advanced metering and Utilities
Reply
Sepehr_Zarrabi
Sepehr_Zarrabi Troubleshooter
Troubleshooter

Posted: ‎2020-04-08 09:01 AM

1 Like
0
2627
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
‎2020-04-08 09:01 AM

Thank you @Charles_Murison. 

 

I also found this bit of information about high-speed logging as it pertains to the LogMode register of the Data Recorder module: 

"For typical logging use, this register does not need to be modified. For continuous high-speed logging (> 1 record per 60 seconds), this register should be set to High Speed Continuous."
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.