Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

how to setup a pulse input from a gas meter into a PM5340

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • how to setup a pulse input from a gas meter into a PM5340
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
kbeal_c-cgroup_
kbeal_c-cgroup_
Explorer

Posted: ‎2025-03-13 11:15 AM

0 Likes
3
917
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
‎2025-03-13 11:15 AM

how to setup a pulse input from a gas meter into a PM5340

Has anyone setup a pulse input on a PM5340 meter?

I have a customer asking if a gas meter pulse can be connected to the status input of the PM5340.

If so, how do you configure the PM5340 to read the pulse input from a gas meter.

Labels
  • Labels:
  • PM5000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Romain_Polette
Romain_Polette Champion
Champion

Posted: ‎2025-03-14 06:12 AM . Last Modified: ‎2025-03-14 06:13 AM

0 Likes
1
881
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
‎2025-03-14 06:12 AM

Hello @kbeal_c-cgroup_ , 

According to user guide, this is not possible to use PM5340 Status Inputs as an external counter.
"Status inputs are typically used for monitoring the status of external contacts or circuit breakers."

 

To configure the Digital Input, please use front face buttons or ION Setup.

Regards, 

Romain POLETTE
Solution Architect - France Operations

See Answer In Context

Reply
Replies 3
Romain_Polette
Romain_Polette Champion
Champion

Posted: ‎2025-03-14 06:12 AM . Last Modified: ‎2025-03-14 06:13 AM

0 Likes
1
882
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
‎2025-03-14 06:12 AM

Hello @kbeal_c-cgroup_ , 

According to user guide, this is not possible to use PM5340 Status Inputs as an external counter.
"Status inputs are typically used for monitoring the status of external contacts or circuit breakers."

 

To configure the Digital Input, please use front face buttons or ION Setup.

Regards, 

Romain POLETTE
Solution Architect - France Operations
Reply
kbeal_c-cgroup_
kbeal_c-cgroup_
Explorer

Posted: ‎2025-03-14 06:38 AM

0 Likes
0
876
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
‎2025-03-14 06:38 AM

Thanks for the response Romain. It looks like I would need a PM8000 with the option board to read a digital input as a pulse for a gas meter.  To bad the PM5340 doesn't have the capabilities of the option board.

Reply
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-03-14 01:10 PM . Last Modified: ‎2025-03-14 01:11 PM

1 Like
0
857
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
‎2025-03-14 01:10 PM

Hi @kbeal_c-cgroup_ 

 

Depending on target costs and other requirements, both PM5500 series as well as PM8000 which have the WAGES monitoring feature can be used.

 

Best Regards,

-Mehran

L3 Expert Advanced metering
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.