Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION9000 Alarm Event Priority

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION9000 Alarm Event Priority
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
AndersDahlskog
AndersDahlskog Contributor
Contributor

Posted: ‎2025-03-17 12:16 AM

0 Likes
1
908
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
‎2025-03-17 12:16 AM

ION9000 Alarm Event Priority

Hi

If alarm priority is set to Info Only for e.g Sag/Swell. Page 184 in user manual 7EN02-0390-08.

Does this effect other functionalities in the meter that is needed to take into consideration ?

 

BR/Anders Dahlskog PAE

Labels
  • Labels:
  • ION Setup
  • ION9000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-03-17 07:10 AM

1 Like
0
883
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
‎2025-03-17 07:10 AM

Hello @AndersDahlskog,

 

Behavior such as waveform capture and logging are not affected by event priority.

The event priority is used to assign a value to the meter's event log and the front panel alarm indicator behavior. Where the priority will affect the meter's event log is if the priority is below the cutoff threshold example Priority=0, the meter will not write events to the meter's onboard event log. The alarm indicator may not indicate an alarm if priority is set to Info Only.

 

If you have software applications such as Power Monitoring Expert the event priority can determine some software behavior.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Reply 1
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-03-17 07:10 AM

1 Like
0
883
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
‎2025-03-17 07:10 AM

Hello @AndersDahlskog,

 

Behavior such as waveform capture and logging are not affected by event priority.

The event priority is used to assign a value to the meter's event log and the front panel alarm indicator behavior. Where the priority will affect the meter's event log is if the priority is below the cutoff threshold example Priority=0, the meter will not write events to the meter's onboard event log. The alarm indicator may not indicate an alarm if priority is set to Info Only.

 

If you have software applications such as Power Monitoring Expert the event priority can determine some software behavior.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.