Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

how to retrieve load profile data to the database

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • how to retrieve load profile data to the database
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
searventz
searventz
Explorer

Posted: ‎2024-10-22 07:46 PM

0 Likes
5
1663
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
‎2024-10-22 07:46 PM

how to retrieve load profile data to the database

I have a PowerlogicION8600, I use ION to retrieve load profile data on a report that is exported to CSV. Then I have a need to save it to a database. How do I retrieve load profile data, especially "kwh del int" in real time every 30 minutes (as in the load profile report) which will be saved to an external database. Because there is no modbus register, and if you add the register tag, it will delete all its data.

Labels
  • Labels:
  • ION Setup
  • PM8000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2024-10-23 08:21 AM

0 Likes
0
1636
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
‎2024-10-23 08:21 AM

Hello @searventz ,

 

One of the many benefits of ION meters is the ability to add customizations. If you want to get interval energy readings like "kWh del int" via modbus, it is possible to add modbus slave module and link the outputs of specific integrator modules to inputs of the Modbus slave module. Then in the setup registers for the modbus slave module you would select the desired format of the registers as well as the starting register. After changes are sent to the meter, you can now read kwh del int values via modbus.

 

One item to note is that interval energy readings will reset at the end of each interval, it can be tricky to catch the reading so close to the end. One suggestion would be to use a store module that can keep the kwh Del for the previous interval. At the end of an interval, have the store module update kwh reading before the integrator is reset. Then link the output of the store module to modbus slave module. What you would then read via modbus is the kwh for the last interval.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 5
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2024-10-23 08:21 AM

0 Likes
0
1637
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
‎2024-10-23 08:21 AM

Hello @searventz ,

 

One of the many benefits of ION meters is the ability to add customizations. If you want to get interval energy readings like "kWh del int" via modbus, it is possible to add modbus slave module and link the outputs of specific integrator modules to inputs of the Modbus slave module. Then in the setup registers for the modbus slave module you would select the desired format of the registers as well as the starting register. After changes are sent to the meter, you can now read kwh del int values via modbus.

 

One item to note is that interval energy readings will reset at the end of each interval, it can be tricky to catch the reading so close to the end. One suggestion would be to use a store module that can keep the kwh Del for the previous interval. At the end of an interval, have the store module update kwh reading before the integrator is reset. Then link the output of the store module to modbus slave module. What you would then read via modbus is the kwh for the last interval.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
searventz
searventz
Explorer

Posted: ‎2024-10-24 08:29 PM

0 Likes
3
1595
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
‎2024-10-24 08:29 PM

Hello @Charles_Murison ,

Thank you for your answer. I will try it later because I am still learning the function of the modules. But is there any other way besides using modbus?

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2024-10-25 08:46 AM

0 Likes
2
1578
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
‎2024-10-25 08:46 AM

Hello @searventz ,

 

For real time communications to your ION8600 meter, your options are ION, modbus, DNP3. Note that ION8600 meters are considered obsolete so there is limited options.

 

Regards,

Charles 

L4 Prime for Advanced metering and Utilities
Reply
searventz
searventz
Explorer

Posted: ‎2024-10-27 07:23 PM

0 Likes
1
1544
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
‎2024-10-27 07:23 PM

Hello @Charles_Murison 

 

sorry, apparently I saw it wrong. the correct type is PowerLogic8650. Is it the same?

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2024-10-28 07:07 AM

0 Likes
0
1529
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
‎2024-10-28 07:07 AM

Hello @searventz ,

 

The ION8650 meter is supported. The answer to what real time communication options are available does not change.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.