Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

alarms/events on cm4 with ionsetup

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • alarms/events on cm4 with ionsetup
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
sesa272464
sesa272464 Leader
Leader

Posted: ‎2015-04-21 08:36 AM . Last Modified: ‎2020-04-22 01:44 AM

0 Likes
7
2213
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
‎2015-04-21 08:36 AM

alarms/events on cm4 with ionsetup

ive been noticing that loading templates with alarm settings won't work all the time.

 

the only way I can get the changes to save and send is if I change the parameters one at a time... such as just change under Van.. hit ok then hit send

 

if I make more than 1 change and hit ok and then try to hit send. it will just get stuck and won't start the downloading process.

 

ive been using the last few versions of ion setup.

 

I noticed this before a while back but the latest version back then solved the problem but now im back to the same issue again.

 

anyone else experiencing the same problem?

Labels
  • Labels:
  • ION Setup
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 7
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2015-04-21 09:06 AM

0 Likes
6
2165
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
‎2015-04-21 09:06 AM

Hi Simon,

Are you experiencing these difficulties just through the Load Template setup function or even using the OnBoard Alarms/Events setup dialog?  What build of ION Setup are you using (the latest can be found here)?  I recently made changes to the Save Template function which had an issue with saving templates so you might want to try downloading the latest, save the file again and then see if you can paste it to another device.

If you are still experiencing issues, please send via e-mail a copy of the MCF file you are sending, details on the CM4 (OS version, model, options, etc.) and a copy of the TEMPLATE.LOG file after you've attempted to paste the MCF file to the MCF with the latest version and I'll look into it.

Reply
sesa272464
sesa272464 Leader
Leader

Posted: ‎2015-04-21 09:23 AM

0 Likes
5
2165
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
‎2015-04-21 09:23 AM

The issue is with both

loading templates don't work.

using the onboard alarms / events setup dialog works ONLY if I make a single change. If I make more than 1 change after I hit the OK button and then hit SEND. the setup dialog closes on its own OR it just freezes for a while. If I hit it a second time it looks like it downloads it to the meter. However after several minutes I would go back and check and those settings didn't stay.

I was using a version before the latest one you release on 4/17. I am having issues with both.

Attachments
4250 alarms.mcf.zip
TEMPLATE.LOG.zip
Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2015-04-21 10:15 AM

0 Likes
4
2165
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
‎2015-04-21 10:15 AM

Looks like the meter is running slightly older firmware (15.030) and there might be a some issue with the actual device (I'll look into this further).  Could you please try and confirm the following:

    1. Is the device in a warm environment (above room temperature)?
    2. If you examine the serial number from the front panel display (Diagnostics -> Meter Information), does the SN# shown stay static or does it mysteriously fluctuate?

One possible solution is to upgrade the meter to the latest firmware (16.010) using DLF-3000 and seeing if the issue is resolved.

Reply
sesa272464
sesa272464 Leader
Leader

Posted: ‎2015-04-21 11:57 AM

0 Likes
3
2165
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
‎2015-04-21 11:57 AM

do you have a link for the latest FW?

I don't have access to the meter front display at the moment

Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2015-04-21 01:18 PM

0 Likes
2
2165
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
‎2015-04-21 01:18 PM

I've put a copy of the latest CM firmware on Box.

You'll also need DLF-3000 as well to do the upgrade which should be available on www.powerlogic.com someplace.

Reply
sesa272464
sesa272464 Leader
Leader

Posted: ‎2015-04-21 01:21 PM

0 Likes
1
2165
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
‎2015-04-21 01:21 PM

thanks - ill give that a try. the latest OS wasn't on powerlogic.com didn't know where else to look.

should I continue to use DL 12.3 as well?

Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2015-04-21 01:36 PM

0 Likes
0
2165
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
‎2015-04-21 01:36 PM

I've placed the latest DL firmware in the same folder (13.0)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.