Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
2014-03-2606:56 PM
Hi Philippe,
As I know the sampling rate of PM3200 range is 32 samples per cycle(20ms for 50Hz or 17ms for 60Hz), so generally I think the sampling rate is fast enough for a 150ms current.
But about the Min/Max values there is a paragraph as following, the Min/Max values are recorded according to the measurements updated every second.
So I don't think PM3200 can always get the Min/Max values for a 150ms reading unless these two times are in the overlap.
Link copied. Please paste this link to share this article on your social media post.
2014-03-2712:14 AM
Hi Pengbin,
Thank you for your answer!
Can anyone explain why the sampling rate is 32 samples per cycle when the PM3200 only shows and registers the value (seen) each second? Then a sampling rate of 1 per second would be sufficient.