Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Schneider Electric Community
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
  • About sesa207393_brid
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
sesa207393_brid
sesa207393_brid
Contributor
‎2026-03-26
31
Posts
7
Likes Received
3
Likes Given
1
Solution

Community Badges

Open Hailing Frequencies - L3
Resistance is Futile - L3
Live Long and Prosper - L2
Open Hailing Frequencies - L2
+7
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
sesa207393_brid
sesa207393_brid Contributor

How the ION7650 "Detect waveshape changes" and "Record ultra-fast elec...

Dear all,In the functions and characteristics datasheet of ION7550/ION7650, I can find the following functions, but how to realize in ION7550 or ION76...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2018 1 3

2014-03-11 01:27 AM

sesa207393_brid
sesa207393_brid Contributor

Can I use the digital and relay outputs of PM5000 for low level switch...

Dear all,Is there any IEC or other standards for the electrical function of power meters?Now I want to use the digital and relay outputs of PM5000 for...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
818 0 0

2014-02-24 11:24 PM

sesa207393_brid
sesa207393_brid Contributor

How much current the iEM3100 models can withstand shortly and continuo...

Dear all,As we know, the iEM3100 models can be used for up to 63A direct measurement, generally there are overload capacity parameters for the meters ...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
742 0 0

2014-02-24 10:29 PM

sesa207393_brid
sesa207393_brid Contributor

Can I replace the standard communication card of an ION7650 so that th...

Hello all,Please help to give your comments, thanks!My question is that whether all of the ION7650 meters have the same motherboard and whether the co...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2492 1 6

2014-02-11 11:58 PM

sesa207393_brid
sesa207393_brid Contributor

Is the Power factor sign convention Chart wrong in PM800 user manual

Hello everyone,In the Power factor sign convention chart for PM800, it shows that in quadrant 2, the load is capacitive and the load in quadrant 3 is ...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1594 1 2

2013-11-29 05:04 AM

Activity Feed
  • Got a Like for Re: What is the sampling rate of a PM3200?. ‎2018-09-13 02:21 AM
  • Got a Like for Can I replace the standard communication card of an ION7650 so that the meter can realize ethernet communication?. ‎2016-04-05 07:29 AM
  • Posted Re: PM5300 vs 5560 - 3-wire RS485 wiring differences? on Metering & Power Quality. ‎2014-09-17 01:29 AM
  • Posted Re: What is the sampling rate of a PM3200? on Metering & Power Quality. ‎2014-03-26 06:56 PM
  • Got a Like for How the ION7650 "Detect waveshape changes" and "Record ultra-fast electrical parameters every 100 ms or every cycle"?. ‎2014-03-25 07:02 AM
  • Posted Re: How the ION7650 "Detect waveshape changes" and "Record ultra-fast electrical parameters every 100 ms or every cycle"? on Metering & Power Quality. ‎2014-03-13 06:05 PM
  • Posted How the ION7650 "Detect waveshape changes" and "Record ultra-fast electrical parameters every 100 ms or every cycle"? on Metering & Power Quality. ‎2014-03-11 01:27 AM
  • Posted Can I use the digital and relay outputs of PM5000 for low level switching input? Can I use the digital outputs to control electromechanical relays which have high inrush current when closing? on Metering & Power Quality. ‎2014-02-24 11:24 PM
  • Posted How much current the iEM3100 models can withstand shortly and continuously?Permissible overload capacity on Metering & Power Quality. ‎2014-02-24 10:29 PM
  • Got a Like for Re: Can I replace the standard communication card of an ION7650 so that the meter can realize ethernet communication?. ‎2014-02-13 03:51 AM
  • Posted Re: Can I replace the standard communication card of an ION7650 so that the meter can realize ethernet communication? on Metering & Power Quality. ‎2014-02-12 05:11 PM
  • Posted Can I replace the standard communication card of an ION7650 so that the meter can realize ethernet communication? on Metering & Power Quality. ‎2014-02-11 11:58 PM
  • Got a Like for Is the Power factor sign convention Chart wrong in PM800 user manual. ‎2013-12-02 06:16 AM
  • Posted Is the Power factor sign convention Chart wrong in PM800 user manual on Metering & Power Quality. ‎2013-11-29 05:04 AM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.