Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Can I use the digital and relay outputs of PM5000 for low level switching input? Can I use the digital outputs to control electromechanical relays which have high inrush current when closing?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Can I use the digital and relay outputs of PM5000 for low level switching input? Can I use the digital outputs to control ele...
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Metering & Power Quality
Start a Topic
sesa207393_brid
sesa207393_brid Contributor
Contributor

Posted: ‎2014-02-24 11:24 PM

0 Likes
0
816
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
‎2014-02-24 11:24 PM

Can I use the digital and relay outputs of PM5000 for low level switching input? Can I use the digital outputs to control electromechanical relays which have high inrush current when closing?

Dear all,

Is there any IEC or other standards for the electrical function of power meters?

Now I want to use the digital and relay outputs of PM5000 for PLC input application, generally the PLC inputs need low level switching input, and the rated current is lower than 10mA, but there is no parameters clarifying the Minimum load of the outputs in the technical documents of PM5000 and other meters, so is there any reference?

The load capacity of PM5000's digital outputs is low ( 20mA and 125mA),we know there will be a high inrush current when energizing AC electromechanical relays and contactors,  so can I use these outputs to control electromechanical relays and contactors? Will it be safe for the controlling and the meter's outputs?

Thanks!

Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.