Posted: 2015-02-25 12:40 AM
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
Accepted Solutions
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
Energy Value will reset at : 9,223,372,036,854,775,807 Wh. In the display screen it will change automatically to Twh or Gwh..
Regards,
Kamal Kumar
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
As per register details the range is up to 1.798*10^308
Posted: 2015-02-25 09:45 PM
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
Thanks Pradip
but for the display on screen, will it change to TWH after GWH?
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
Hi Kamal, is this value the same for all PM5000 (51, 53, 55xx) and PM5350? Thanks!
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
Hi Daniel,
Yes, this Energy value is common for all PM5000 series ( 51xx,53xx, 55xx) and PM5350 also.
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
Hi @Kamal,
If the max. reading is 9,223,372,036,854,775,807 Wh, which means the unit is PWh? Never seen this unit on power meter before so would like to confirm with you. Thanks