Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
2024-02-0710:20 AM
Unable make Telnet connection to ION8650
Hello SE support,
I am unable to make the telnet connection to a ION8650 meter, and got error message: "Could not open connection to the host, on port 23: Connect Failed."
check the comm module, can't see if telnet port is enable or not:
For ION8650 meters with firmware V4.40.1or higher, Telnet and FTP protocols are no longer supported, and you can login to the meter through SSH. For lower versions you can telnet to the meter.
For ION8650 meters with firmware V4.40.1or higher, Telnet and FTP protocols are no longer supported, and you can login to the meter through SSH. For lower versions you can telnet to the meter.