Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84589members
353854posts

PM8000 analog output configuration

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
sesa191869
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
228

PM8000 analog output configuration

Hello,

Can you tell me how to configure option module analog ouput of PM8000 using ION Setup?

It is not described well in the user guide, so I was not able to complete.

The customer wants to transfer kW value to 4-20mA analog output, and the maximum value is 150MW.

The problem is that source selection tab is not activated.

Can anyone teach me step by step?

Thank you for your help in advance!

Tags (2)

Accepted Solutions
Yut
Captain
Captain
0 Likes
0
167

Re: PM8000 analog output configuration

Please  see ION Reference study the Analog Output Module. You need ION Setup or Designer to add this module and link the input into the power meter module to get kW.

See Answer In Context

1 Reply 1
Yut
Captain
Captain
0 Likes
0
168

Re: PM8000 analog output configuration

Please  see ION Reference study the Analog Output Module. You need ION Setup or Designer to add this module and link the input into the power meter module to get kW.