Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM5560 Connection Issue with ION Setup

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PM5560 Connection Issue with ION Setup
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
ABDUL8
ABDUL8
Explorer

Posted: ‎2025-08-03 09:51 PM

0 Likes
6
3044
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
‎2025-08-03 09:51 PM

PM5560 Connection Issue with ION Setup

I'm having trouble connecting the PM5560 meter (latest firmware v4.4.8) with ION Setup (v3.2.25185.01) using the Single ION Device Configuration Mode. However, it works fine when I connect to the PM8000 or ION9000. Is this mode only meant for ION devices?  I can still access the meter via the webpage. Any thoughts or advice to get PM5560 working with IONSetup would be much appreciated.

Attachments
Labels
  • Labels:
  • PM5000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Sidharthan
Sidharthan Contributor
Contributor

Posted: ‎2025-08-04 03:51 AM

1 Like
0
3034
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
‎2025-08-04 03:51 AM

Single ION Device Configuration Mode is for ION devices only,

Please follow this FAQ000259425 How to add a device into ION Setup | Schneider Electric India
To add PM5560 device in ION Setup.

See Answer In Context

  • Thumbnail of PowerLogic PM5000 series
    Schneider Electric
    PowerLogic PM5000 series
View products (1)
Tags (1)
  • Tags:
  • Add Ethernet based devices to ION Setup
Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2025-08-07 01:50 PM

0 Likes
1
2983
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
‎2025-08-07 01:50 PM

The PM5560 is not an ION Device (so there is no Setup Assistant).  Almost all Basic Metering offers are Modbus based and do not communicate using ION protocol (which is why Single ION Device mode doesn't work and why there are no Setup Assistant).

See Answer In Context

Reply
Replies 6
Sidharthan
Sidharthan Contributor
Contributor

Posted: ‎2025-08-04 03:51 AM

1 Like
0
3034
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
‎2025-08-04 03:51 AM

Single ION Device Configuration Mode is for ION devices only,

Please follow this FAQ000259425 How to add a device into ION Setup | Schneider Electric India
To add PM5560 device in ION Setup.

  • Thumbnail of PowerLogic PM5000 series
    Schneider Electric
    PowerLogic PM5000 series
View products (1)
Tags (1)
  • Tags:
  • Add Ethernet based devices to ION Setup
Reply
ABDUL8
ABDUL8
Explorer

Posted: ‎2025-08-04 04:23 PM

1 Like
0
3023
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
‎2025-08-04 04:23 PM

Thanks, Sidharthan it works.

Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2025-08-05 04:19 PM

1 Like
0
3008
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
‎2025-08-05 04:19 PM

The "Single ION Device Configuration mode" as stated in the name is for ION Device only (otherwise I would of called it just "Single Device Configuration mode").

Most Basic Meter products (like the PM5000 series) are Modbus based and would also require either a port selection option to be available (since most use port 502 instead of port 7700/7443) or slow down scanning as it would have to alternate between ION and Modbus protocols when done serially (modems are not even viable using Modbus connections).

Reply
ABDUL8
ABDUL8
Explorer

Posted: ‎2025-08-06 10:32 PM . Last Modified: ‎2025-08-06 10:35 PM

0 Likes
0
2994
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
‎2025-08-06 10:32 PM

Thanks, Robert and Sidhartan.
Another issue I’ve encountered is when I add the PM5560 in ION Setup—it only shows the advanced settings, and the setup assistant icon disappears.

 Screenshot 2025-08-07 125418.pngIs there any way to get the setup assistant to appear?

Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2025-08-07 01:50 PM

0 Likes
1
2983
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
‎2025-08-07 01:50 PM

The PM5560 is not an ION Device (so there is no Setup Assistant).  Almost all Basic Metering offers are Modbus based and do not communicate using ION protocol (which is why Single ION Device mode doesn't work and why there are no Setup Assistant).

Reply
ABDUL8
ABDUL8
Explorer

Posted: ‎2025-08-07 04:22 PM

0 Likes
0
2978
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
‎2025-08-07 04:22 PM

Thanks Robert, that explains!
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.