Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84570members
353841posts

PM3255 - Log Configuration in ION Setup

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
JamesAZZO
Sisko | EcoXpert Master Sisko | EcoXpert Master
Sisko | EcoXpert Master
0 Likes
2
481

PM3255 - Log Configuration in ION Setup

In order to enable the Energy and Demand logs of the PM3255, you have to use the front panel of the meter. You cannot configure the log enable/disable from ION Setup. Can someone explain why this is?

Also, can someone like confirm that with the new firmware of the PM3255, we can configure the new user-definable logs in ION Setup and from what firmware this is supported?

I posted this in the hardware area, as it will be the most common place for this to be found, but is also a related forum.

Tags (3)

Accepted Solutions
Robert_Lee
Captain Captain
Captain
0 Likes
1
307

Re: PM3255 - Log Configuration in ION Setup

According to the latest iEM3000 Users Guide, those devices still do not support a Modbus command to configure the data logging capabilities of those models (located in Chapter 5).  Until the firmware is modified to support both the reading and writing of the data log configuration, ION Setup won't be able to do anything to configure the data logging.

See Answer In Context

2 Replies 2
Robert_Lee
Captain Captain
Captain
0 Likes
1
308

Re: PM3255 - Log Configuration in ION Setup

According to the latest iEM3000 Users Guide, those devices still do not support a Modbus command to configure the data logging capabilities of those models (located in Chapter 5).  Until the firmware is modified to support both the reading and writing of the data log configuration, ION Setup won't be able to do anything to configure the data logging.

JamesAZZO
Sisko | EcoXpert Master Sisko | EcoXpert Master
Sisko | EcoXpert Master

Re: PM3255 - Log Configuration in ION Setup

Ahh. I figured as much Robert, hence posting in the hardware area and tagging Marc. This is a problem for our sites where the boards are remote and we need to change log settings.

Cheers,

James