Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84321members
353479posts

Modbus Registries ION 7350

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
JonMiles
Lieutenant | EcoXpert Master Lieutenant | EcoXpert Master
Lieutenant | EcoXpert Master
0 Likes
3
478

Modbus Registries ION 7350

Does anybody know the ION registries used to switch the digital output 1 & 2 after configuration in Designer to D01 and D02?

 

Thanks,

Jon


Accepted Solutions
JonMiles
Lieutenant | EcoXpert Master Lieutenant | EcoXpert Master
Lieutenant | EcoXpert Master
0 Likes
0
375

Re: Modbus Registries ION 7350

Now resolved, It was the external pulse tied to the modbus address 42020 for external pulse 20.

Thanks for the help,

Jon

See Answer In Context

3 Replies 3
Charles_Murison
Picard Picard
Picard
0 Likes
0
375

Re: Modbus Registries ION 7350

Not sure what you mean by "switch", toggle the state of the output, change the label?

Second, heading is asking modbus register, question is asking ION register. There is a difference.

L4 Prime for Advanced metering and Utilities
jimbradley
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
375

Re: Modbus Registries ION 7350

Doing Modbus writes to a ION meter is a little tricky.

You can only do writes to a set of External modules.  I believe the map is fixed

You have to link an External Boolean module or an External Pulse Module to the DO Module.

It's documented "somewhere" so have a look at the Modbus doc for ION or check the Knowledge base.

Jim

JonMiles
Lieutenant | EcoXpert Master Lieutenant | EcoXpert Master
Lieutenant | EcoXpert Master
0 Likes
0
376

Re: Modbus Registries ION 7350

Now resolved, It was the external pulse tied to the modbus address 42020 for external pulse 20.

Thanks for the help,

Jon