Ask our Experts
Didn't find what you are looking for? Ask our experts!
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
I have two ION7650 on 11kV supplies.
My client wants to know when a sag or swell waveform capture has occured in the meter by receiving a notification in the site BMS using a Modbus register as the trigger.
Using Designer, I have looked at a Modbus Slave module linked to the output of the Sag/Swell module (DistState) to change the value in the slave register from 0 to 1 (Packed Boolean). Will the Manual Waveform Trigger in PME simulate an output on the Sag/Swell module?
Is this the best way to go about this or is there a better solution?
Link copied. Please paste this link to share this article on your social media post.
Hi
A manual waveform trigger won't stimulate a sag/swell output, but one idea would be to pulse merge a manual waveform trigger with the sag/swell output and link that to a counter module. The counter module output can then be exposed to modbus which helps prevent any sags/waveforms being missed by a polling approach (the counter is the absolute number of changes).
BR
Tom
Link copied. Please paste this link to share this article on your social media post.
One way I have also seen this done is linking the Sag/swell count to a modbus register, then BMS system is configured to recognize a change in value to indicate a sag or swell. Another option would be to link the sag/swell end pulse to a one shot timer that can then be linked to a mobus register. Oneshot period would have to be greater than the modbus polling period. The sag/swell state could change values so fast the modbus poll could miss the event.
Link copied. Please paste this link to share this article on your social media post.
Hi
A manual waveform trigger won't stimulate a sag/swell output, but one idea would be to pulse merge a manual waveform trigger with the sag/swell output and link that to a counter module. The counter module output can then be exposed to modbus which helps prevent any sags/waveforms being missed by a polling approach (the counter is the absolute number of changes).
BR
Tom
Link copied. Please paste this link to share this article on your social media post.
One way I have also seen this done is linking the Sag/swell count to a modbus register, then BMS system is configured to recognize a change in value to indicate a sag or swell. Another option would be to link the sag/swell end pulse to a one shot timer that can then be linked to a mobus register. Oneshot period would have to be greater than the modbus polling period. The sag/swell state could change values so fast the modbus poll could miss the event.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.