Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION7650 - Configuring Watchdog and Event present digital outputs

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • ION7650 - Configuring Watchdog and Event present digital outputs
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
sesa207714_brid
sesa207714_brid Leader
Leader

Posted: ‎2016-02-11 02:26 AM

0 Likes
1
1245
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
‎2016-02-11 02:26 AM

ION7650 - Configuring Watchdog and Event present digital outputs

Hi,

Has anyone configured the digital outputs on the ION7650 for either a watchdog, or an Alarm/Event being present on the system?

Currently the customer has asked for the ION meters to be configured with a Watchdog/health contact. This will stay closed until the meter loses power, then it should reopen. I'm assuming it would be easily achieved using the solid state digital outputs, but I have no way off testing it as the customer does not want to power the meter down.

In regard to the event present output, I wave looked and noticed that there are a lot of statuses for when waveforms have been captured that can be ORed together in the VIP frameworks for the meter, but there does not seem to be any single status for when the meter has captured an alarm/event or waveform. Is this correct, or have i missed this signal somewhere?

Thanks for all of your assistance.

Regards,

Martin

Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Yut
Yut
Leader

Posted: ‎2016-02-14 07:59 PM

0 Likes
0
1193
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
‎2016-02-14 07:59 PM

To indicate that the meter is ON please take a look at the Diagnostics module there is one output called Power Up Pulse you can use it to trigger the Force On input of the Digital Output assigned to one of the three output mechanical relays the  set up for digital out put Polarity must be Inverted when power up the state of the relay will change when power down the relay will drop.

For the Sag/Swell and Transient module there some status and trigger output which you can use as alarm. But do not use the meter as relay especially when some customer ask for DNP signal called Unsolicited Response in ION meter this function always disabled.

See Answer In Context

Reply
Reply 1
Yut
Yut
Leader

Posted: ‎2016-02-14 07:59 PM

0 Likes
0
1194
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
‎2016-02-14 07:59 PM

To indicate that the meter is ON please take a look at the Diagnostics module there is one output called Power Up Pulse you can use it to trigger the Force On input of the Digital Output assigned to one of the three output mechanical relays the  set up for digital out put Polarity must be Inverted when power up the state of the relay will change when power down the relay will drop.

For the Sag/Swell and Transient module there some status and trigger output which you can use as alarm. But do not use the meter as relay especially when some customer ask for DNP signal called Unsolicited Response in ION meter this function always disabled.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.