Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84827members
354281posts

How much current the iEM3100 models can withstand shortly and continuously?Permissible overload capacity

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

sesa207393_brid
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
118

How much current the iEM3100 models can withstand shortly and continuously?Permissible overload capacity

Dear all,

As we know, the iEM3100 models can be used for up to 63A direct measurement, generally there are overload capacity parameters for the meters which measure current though CTs, so do the iEM3100 models also have these parameters?

Now I want to use iEM3150 for motor's measures, but because there will be a high inrush current when AC motor is energized directly, the value can be 5~7In and maybe even larger, so can I use iEM3150 for motors? If yes, what's the max. power is permissible?

Thanks!