Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84863members
354351posts

Firmware on ION7350 Ethernet

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
jlin_dvlnet_com
Ensign
Ensign
0 Likes
1
177

Firmware on ION7350 Ethernet

Hello,

Is it possible to flash an ethernet ION7350 with non-ethernet firmware such that it opens COM2 for any protocol (rather than being limited to ethergate)?  We are not using the ethernet port at all.

Thanks,

Jason

Tags (2)

Accepted Solutions
jlin_dvlnet_com
Ensign
Ensign
0 Likes
0
155

Re: Firmware on ION7350 Ethernet

Tech support notified me that the ethernet port is hard-coded into the meter, so this is not an option.

The alternative is to use an ethernet-to-serial gateway.

See Answer In Context

1 Reply 1
jlin_dvlnet_com
Ensign
Ensign
0 Likes
0
156

Re: Firmware on ION7350 Ethernet

Tech support notified me that the ethernet port is hard-coded into the meter, so this is not an option.

The alternative is to use an ethernet-to-serial gateway.