Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
Hello,
We had a PME training and the trainer used an 8650B simulator for some of the training. He was able to connect to this virtual meter using ION Setup and PME. Could I please have some guidance for getting this setup?
All I can remember was him starting the simulator and being able to connect to it using an IP address of 255.255.255.0 or something similar. I'm sure I am missing a step or maybe have the default IP address wrong? Any tips would be appreciated.
Thank you,
Brandon
Link copied. Please paste this link to share this article on your social media post.
The Windows simulators use localhost (127.0.0.1)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Good day kindly refer to the solution posted the solution also works in PME, but there seems to be a problem when connecting in Windows Server 2022 with PME, awaiting updates
Life Is On 🙂
Link copied. Please paste this link to share this article on your social media post.
Hello,
I was able to connect the device using the (127.0.0.1) localhost, but while using multiple simulators (ION7400,PM8000 AND ION8650) I´m running into issues while connecting each device to the PME since I´m not sure how this process works, when I open the simulators and then open the web applications on PME they all connect to one same simulator, even tho I created on the manager console one for each simulator. Does anyone know how can I connect multiple simulators on PME? Also i was trying to find the historical data of the simulator but I can´t see any historical register data, is it possible to read historical data from a simulator device? Thank you in advance.
Link copied. Please paste this link to share this article on your social media post.
Hello @Jorge_Pasamar ,
Different versions of simulator may have different behavior. By default, simulator will use port 7700 on computer running simulator. Some versions of simulator would increment by 1 each time if port already in use, 7701, 7702, for example. Some simulators could have the ION port defined with argument, simulator.exe -p [port number desired] . In PME, would need to define the port to match the simulator.
Regards,
Charles
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.