Can PM8000 4-wire card (METSEPMRS4854W) communicate PowerLogic protocol.
Metering & Power Quality
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
2023-10-2306:08 AM
Can PM8000 4-wire card (METSEPMRS4854W) communicate PowerLogic protocol.
I have some daisy-chains of Digitrip 810D's that are currently communicating via PowerLogic (Sy/Max) protocol to PME. These are communicating via various gateways (EGX100, EGX200, LINK150, etc.). I understand that the last gateway to communicate PowerLogic protocol is the LINK150 that is due to be discontinued. It is also the last to have 4-wire RS-485 support. Can I use the PM8000/ION9000 4-wire module (METSEPMRS4854W) as a gateway for the downstream Digitrip 810D's? What communication settings should I use in the PM8000 if this is possible? Thank you in advance for your assistance.