Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM8000 ring topology RSTP

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PM8000 ring topology RSTP
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
NicoleTang
NicoleTang Contributor
Contributor

Posted: ‎2023-10-18 03:38 PM

0 Likes
1
1880
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
‎2023-10-18 03:38 PM

PM8000 ring topology RSTP

Hi everyone.

I have read few forums in here in regards to RSTP or ring topology on PM8000 meters.

I am still not sure from the forums whether RSTP has been implemented successfully on site.

I have a site that has just been upgraded to Cisco managed switches, and we have PM8000 meters on site that are daisy-chained in a ring, back to the switch (to occupy 2 ports).

There are 3 loops, and one loop consists of 4 PM8000 meters, another of 5, and another of 10 PM8000.

The meters are connected to just the dedicated VLAN and the meters RSTP are enabled also.

First 2 loops of 4 and 5 PM8000s were connected as a ring without issue. The last loop of 10 PM8000 caused a network wide shutdown. 

I want to know if there is:

1. a limit or number of PM8000 that can be daisy chained in a ring

2. a prefer or specific RSTP or STP protocol to use that works with PM8000

3. maybe firmware fix released? The meters are by the customer and I noticed they varied in firmware from the menus

 

Appreciate technical advice. Thanks.

Attachments
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2023-10-19 09:02 AM . Last Modified: ‎2023-10-19 09:03 AM

1 Like
0
1868
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
‎2023-10-19 09:02 AM

Hello @NicoleTang ,

 

1. a limit or number of PM8000 that can be daisy chained in a ring
CM: There is more of a performance limitation rather than protocol limitation. As you increase the number of devices, the amount of time for network to settle when there is a change takes longer.

2. a prefer or specific RSTP or STP protocol to use that works with PM8000
CM: RSTP is the protocol PM8000 meters support. 

3. maybe firmware fix released? The meters are by the customer and I noticed they varied in firmware from the menus
CM: There were changes to RSTP on the meters around the V2.2.0 time range. If you meter is V3.0.0 or newer firmware should not be a factor.

Be sure the meters and switches have RSTP enabled before connecting the meters in a loop. If loop is made before RSTP is enabled, the network will see a storm of traffic and likely have networks not happy.

 

Regards,

Charles

 

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Reply 1
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2023-10-19 09:02 AM . Last Modified: ‎2023-10-19 09:03 AM

1 Like
0
1868
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
‎2023-10-19 09:02 AM

Hello @NicoleTang ,

 

1. a limit or number of PM8000 that can be daisy chained in a ring
CM: There is more of a performance limitation rather than protocol limitation. As you increase the number of devices, the amount of time for network to settle when there is a change takes longer.

2. a prefer or specific RSTP or STP protocol to use that works with PM8000
CM: RSTP is the protocol PM8000 meters support. 

3. maybe firmware fix released? The meters are by the customer and I noticed they varied in firmware from the menus
CM: There were changes to RSTP on the meters around the V2.2.0 time range. If you meter is V3.0.0 or newer firmware should not be a factor.

Be sure the meters and switches have RSTP enabled before connecting the meters in a loop. If loop is made before RSTP is enabled, the network will see a storm of traffic and likely have networks not happy.

 

Regards,

Charles

 

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.