Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84269members
353375posts

Can I replace the standard communication card of an ION7650 so that the meter can realize ethernet communication?

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
sesa207393_brid
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Can I replace the standard communication card of an ION7650 so that the meter can realize ethernet communication?

Hello all,

Please help to give your comments, thanks!

My question is that whether all of the ION7650 meters have the same motherboard and whether the communication card can be replaced with any other one according to customer‘s requirement?

Thanks!


Accepted Solutions
sesa50168
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: Can I replace the standard communication card of an ION7650 so that the meter can realize ethernet communication?

Yes, the communications card can be changed.  There are multiple options available, and they are listed in the catalog.  For example, the card which includes the standard communications plus 10Base-T/100Base-TX Ethernet, is the P765CE0A.

See Answer In Context

6 Replies 6
sesa50168
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: Can I replace the standard communication card of an ION7650 so that the meter can realize ethernet communication?

Yes, the communications card can be changed.  There are multiple options available, and they are listed in the catalog.  For example, the card which includes the standard communications plus 10Base-T/100Base-TX Ethernet, is the P765CE0A.

sesa207393_brid
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: Can I replace the standard communication card of an ION7650 so that the meter can realize ethernet communication?

Thank you very much John!

So if there is an ION7650 equipped with a standard communication card, I can order a new communication card which includes the standard communications plus 10Base-T/100Base-TX Ethernet to replace the standard one. Is my understanding right? Thanks!

JamesAZZO
Sisko | EcoXpert Master Sisko | EcoXpert Master
Sisko | EcoXpert Master
0 Likes
0
502

Re: Can I replace the standard communication card of an ION7650 so that the meter can realize ethernet communication?

Yup. Do it sometimes for various reasons. Excellent option the I/O module can be added too, FYI.

sesa12425_bridg
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
2
502

Re: Can I replace the standard communication card of an ION7650 so that the meter can realize ethernet communication?

Hi John,

May I know the procedure how to do the change after buying the module? Do you have any PDF? Can it be replaceable at site?

Thanks.

Yut
Captain
Captain
0 Likes
1
502

Re: Can I replace the standard communication card of an ION7650 so that the meter can realize ethernet communication?

Document 70052-0252-00 I think you can download at the product web page.

sesa252887_brid
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
502

Re: Can I replace the standard communication card of an ION7650 so that the meter can realize ethernet communication?

Hi

If I would like to have one RS485 COM and Ethernet RJ45 port at the same time, P765CE0A is the right option?

Thanks

Ken HSU

Regards,

Abon