Calculating Logging Storage Length in the PM5560 Datalog 1
Is there a simple formula for calculating how many days of logging is available in Datalog #1 when configured at 5 minute intervals and all 16 channels of logs are used?
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
Hi James,
The maximum log size for the PM556x (PM5560, PM5561 and PM5563) is 35040 records total.
In your scenario: the number of records, N=16 and the logging frequency: f = 5min intervals or 12 readings/hour
The number of records per day is R = N*f*24 = 16*12*24 = 4608 records/day
The total number of days, with this scenario, is 35040/R = 35040/4608 = 7.6 days or 7d 14h 30m
If you are logging at this rate, I would suggest having some supervisory system (like StruxureWare PowerSCADA Expert or StruxureWare Power Monitoring Expert) to poll the meter to ensure a contiguous database.
If I can ask, What scenario or system are you configuring the PM556x (in this way) for ?
Kind Regards,
Chris.
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
We will have PME, but requirements are 2 weeks onboard logging as it's a remote site and connection by 3G isn't always reliable there.
5 min logs is because of solar sources being measured. Cloud cover changing makes fast changes we want to see over 5 minutes.
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
Hi James,
What are the 16 parameters you are wanting to record at this rate ? Can you share how you might prioritize them ?
Best Regards,
Chris.
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
- Real Energy Into the Lord
- Real Energy Out of the Load
- Demand Real Power Total
- Real Power Total
- Real Power A
- Real Power B
- Real Power C
- Reactive Power Total
- Apparent Power Total
- Power Factor Sign Total
- Vln avg
- Vln avg
- I avg
- THD V1
- THD V2
- THD V3
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
James, the maximum number of values you can record is 14, not 16. We are working on a spreadsheet that will automatically calculate how many days of logs you will have, based on the parameters you select and the frequency of logging. I will send you a draft version and we will publish after it's validated.
And you should be able to log 14 values every 5 minutes for around 50 days.
Let me know if questions.
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
Is it well understood that there can be saved over 200.000 logs in PM5561?
If the formula in the first answer is right, the capacity will be 201.600?
the leaflet says: 6 parameters for 90 days with 15 munutters interval.
Can you help find the accurate logging calculation? 🙂
Best regards
Michael Thode
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
There has been a similar thread [DEAD LINK /message/16555#16555]https://powersolutionscommunity.schneider-electric.com/message/16555#16555. When I use the datalog calculator (spreadsheet from Daniel) I get 55 days for 14 parameters with 5 minutes interval
Regards
Daniel
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
James, is possible Log THD Data?
Im trying with ION Setup but dont appear this parameter.
Regards!
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
This could be a very valuable spreadsheet for me. Its been a couple of year since you posted this, so I may guess the spreadsheet is done? haha.. Talking seriously, can someone give me a link to download the spreadsheet? Where can i find it? Since it is not in this thread.
Thanks!