Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
I have installed build v3.0.17307 of ION Setup (after uninstalling a most recent version v3.0 18124).
Installation is OK but when I launch ION Setup I got this error msg window.
"Unable to initialize COM library".
Any help ?
I need the 17307 build because this is the version compatible with the FW upgrade feature for the new Power Solution product IFL12-H (developped in India).
Thanks.
Link copied. Please paste this link to share this article on your social media post.
Answer I got from Robert Lee.
"I suspect that error is due to either MS changing something about how the Common Control library is initialized (ION Setup uses that for the Windows File Open/SaveAs dialogs) or some other application is not properly initializing the control when its finished using it. I've only heard of this occurring on certain PCs so something else is likely the cause (you could likely boot that PC in Windows Safe Mode and start that same ION Setup and it would likely run fine).
"
Link copied. Please paste this link to share this article on your social media post.
Answer I got from Robert Lee.
"I suspect that error is due to either MS changing something about how the Common Control library is initialized (ION Setup uses that for the Windows File Open/SaveAs dialogs) or some other application is not properly initializing the control when its finished using it. I've only heard of this occurring on certain PCs so something else is likely the cause (you could likely boot that PC in Windows Safe Mode and start that same ION Setup and it would likely run fine).
"
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.