Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the Schneider Electric Community! We have moved to a new address: community.se.com — bookmark it today and contact SchneiderCommunity.Support@se.com if you have any questions!
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82731members
350480posts

Cybersecurity - What is your competitive advantage of Mercury over other competition office?

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

LinkedInLive_QA
Lieutenant JG
Lieutenant JG
1
1235

Cybersecurity - What is your competitive advantage of Mercury over other competition office?

What is your competitive advantage of Mercury over other competition office?

Tags (1)
1 Reply 1
G_Enigmedia
Ensign
Ensign
0
1234

Re: Cybersecurity - What is your competitive advantage of Mercuri over other competition office?

The main competitive advantage that we have and unique value proposition is that we are able to encrypt communication with the latency below two milliseconds independently on the protocol of the network for any kind of device that we are running.

 

So what does it means? It means that we can easily implement a solution in a field without disrupting the network.

 

Typically, when you are trying to apply the IT techniques to the OT field you have some problems in design. One of those problems for instance is how do you make the secure connections. In the IT the latency for internet is over 100 milliseconds and it is okay because it is designed by humans so you don’t care about the latency below 100 miliseconds.

 

However, a machine has a strict latency requirements so we are solving this technical problem and then we have further benefits and we leverage on this technical benefits on other features.