Posted: 2020-07-03 12:53 PM . Last Modified: 2024-04-08 01:48 AM
Importing manual power measurements
Where is the template excel file on the DCO server for importing manual power measurements ?
(CID:111415448)
- Labels:
-
Data Center Operation
Link copied. Please paste this link to share this article on your social media post.
Accepted Solutions
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
Posted: 2020-07-03 12:53 PM . Last Modified: 2024-04-08 01:48 AM
Hi James,
As illustrated, the template file can be created via: File > Import > "Manual Power Measurements from Excel Workbook", ... "Create template file" feature:
manual import and creating the template file would need that ETL import database has been setup already. It is worth to mention that a template file could be created based on the selected room ("Choose external system") - if the room should contain associated devices (such as PDU getting its measurements from DCE), then those devices may not appear in the template file.
Kind regards
(CID:111415735)
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
Posted: 2020-07-03 12:53 PM . Last Modified: 2024-04-08 01:48 AM
Hi James,
As illustrated, the template file can be created via: File > Import > "Manual Power Measurements from Excel Workbook", ... "Create template file" feature:
manual import and creating the template file would need that ETL import database has been setup already. It is worth to mention that a template file could be created based on the selected room ("Choose external system") - if the room should contain associated devices (such as PDU getting its measurements from DCE), then those devices may not appear in the template file.
Kind regards
(CID:111415735)
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
Posted: 2020-07-03 12:53 PM . Last Modified: 2024-04-08 01:48 AM
Thanks Jef Faridi, have got the template file now.
The documentation on the website seems to suggest the file is already on the DCO server, maybe this could be modified with what you have supplied above.
(CID:111415787)
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
Posted: 2020-07-03 12:53 PM . Last Modified: 2024-04-08 01:48 AM
You are most welcome James,
will be added to our documentation soon - very good suggestion, thank you.
Kind regards
(CID:111937308)
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
Posted: 2020-07-03 12:54 PM . Last Modified: 2024-04-08 01:48 AM
Thanks for pointing out the unclarity in the documentation James. I've updated it to try to explain better that the file is automatically created and includes the current data in your solution on the server when you click Create template file... I hope this clarifies it for you and other users.
Importing manual power measurements
(CID:111937349)
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
Posted: 2020-07-03 12:54 PM . Last Modified: 2024-04-08 01:48 AM
Pernille Bagger Nielsen and Jef Faridi good to see the documentation updated. I have successfully now setup the process and imported power data.
One last thing to note is it would be good on the export/import Excel file to show the connected device on the breaker. So at the moment my file looks like this
It would be good to have another column that said connected device (power consumer) with the name of said device, like in the Breaker Panel tab of a Power Panel
(CID:111937353)
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
Posted: 2020-07-03 12:54 PM . Last Modified: 2024-04-08 01:48 AM
Hi James,
I will capture that as a feature request, thanks.
Kind regards
(CID:111937394)
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
Posted: 2020-07-03 12:54 PM . Last Modified: 2023-10-22 02:42 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.