Posted: 2020-07-05 05:19 PM . Last Modified: 2024-04-03 03:24 AM
ATS' cannot be used to power equipment
We have 2 Switchgear which feed our Cooling Units via an ATS.
Switchgear A and Switchgear B both power the ATS which in turn power the Cooling Unit.
Using the Generic ATS genome, I can set the power dependancy from the ATS to a primary connection of Switchgear A and a secondary connection of Switchgear B, which is great (as previously they could only be powered from one source), however, I am unable to power the cooling unit from the ATS.
The genome suggests that the ATS has a Dist panel, but there are no properties in order to create a distribution panel. Assuming that this is why I can't power the cooling unit?
I have also tried to power single feed devices via an ATS (i.e. a Distribution Board), however am finding similar results. I assume this is due to the lack of a breaker panel in the genome?
(CID:140219010)
- Labels:
-
Data Center Operation
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
Posted: 2020-07-05 05:19 PM . Last Modified: 2024-04-03 03:24 AM
Hi Sean,
I don't think equipment (such as cooling units) can be powered/connected directly to an ATS device (as power supply). You might want to add a PDU between cooling unit(s) and ATS.
Kind regards
(CID:140712759)
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
Posted: 2020-07-05 05:19 PM . Last Modified: 2023-10-20 04:57 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.