Issue
SER8000 series room controllers communications options
Environment
SER8000 series room controllers
Cause
Integration to SER8000 room controllers via Modbus is required.
Resolution
Currently, the SER8000 series room controllers communications options are Zigbee Pro or BACnet MS/TP...