MSMQ issue causes Alarms and Access Event delivery problems between CyberStations

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • MSMQ issue causes Alarms and Access Event delivery problems between CyberStations
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Cody_Failinger
    Cody_Failinger
  • Product_Support
    Product_Support
  • DavidFisher
    DavidFisher
  • AdamSteele
    AdamSteele
  • SangKim
    SangKim
  • CraigEl
    CraigEl
  • AbeMeran
    AbeMeran

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
2976 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

MSMQ issue causes Alarms and Access Event delivery problems between CyberStations

Picard Product_Support
‎2018-09-11 08:51 AM

Last Updated: Administrator CraigEl Administrator ‎2022-08-08 07:59 PM

Issue

Continuum running under MS Windows 7, Vista or MS Windows Server 2008 (including R2)

Access event viewers at workstations other than the primary access server do not show events.

Alarms acknowledged at one CyberStation would remain unacknowledged in the other CyberStations. 

Product Line

Andover Continuum

Environment

  • CyberStation
  • Microsoft Windows 7
  • Microsoft Windows Server 2008
  • Microsoft Windows Server 2008 R2

Cause

Problem in Microsoft MSMQ component.

MSMQ service might not send or receive messages after you restart a computer that is running Windows 7, Windows Server 2008 R2, Windows Vista or Windows Server 2008.

This will cause any Continuum component that uses MSMQ (such as Alarms and Access Events) to fail.

Microsoft has issued a hot fix for this MSMQ problem.

Resolution

Use the following command prompt test to verify the problem
netstat -ano | findstr 1801
The command tests whether MSMQ is listening for messages.

For example, Continuum WS 'A' is the primary access server (PAS) with an Event Viewer 'EV' up,  a second Continuum WS 'B'  is also displaying the same EV.

If MSMQ is functioning normally you should see the following.

1. is the IP address of WS 'B' that has established a link to WS 'A' 

2. is the IP address of WS 'A', the PAS in this case.

2560 is the listening MSMQ process PID 

You can clearly see that there is a MSMQ process (2560) in WS 'B' LISTENING on port 1801

If there is no MSMQ process listening the output of the command will show the loopback or localhost IP address 127.0.0.1

and you have to install the following Microsoft hotfix:

Package:

-----------------------------------------------------------

-----------------------------------------------------------

See Microsoft KB Article Number: 2554746

 

** In very rare occasions, removing MSMQ and adding MSMQ again to the PC is required.

** Once it is re-installed, please refer to Access event viewers running in a workstation other than the Primary Access Server stop displaying e... to set the MSMQ CleanupInterval setting to one hour in the primary access server.

Labels (1)
Labels:
  • Andover Continuum
Tags (1)
  • Find more articles tagged with:
  • 13192
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.