Communications troubleshooting in SmartStruxure

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Communications troubleshooting in SmartStruxure
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • DavidFisher
    DavidFisher
  • Carl_Slack
    Carl_Slack
  • RobertAndriolo
    RobertAndriolo
  • CraigEl
    CraigEl
  • Cody_Failinger
    Cody_Failinger
  • sesa177673
    sesa177673
  • Product_Support
    Product_Support

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
3425 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Communications troubleshooting in SmartStruxure

Picard Product_Support
‎2018-09-11 08:49 AM

Last Updated: Administrator CraigEl Administrator ‎2022-08-08 06:29 PM

Issue

The built in logs for troubleshooting communications from SmartStruxure ES/AS to SmartStruxure ES/AS remove the need for network captures for SmartStruxure communications. However, SmartStruxure to BACnet continues to be ideal for traditional means of network captures. The most common capture method is Wireshark when dealing with BACnet device to BACnet device communication.

Product Line

EcoStruxure Building Operation

Environment

  • SmartStruxure
  • BACnet
  • ES
  • AS

Cause

The need to troubleshoot communications issues from device to device whether this is ES to AS or vice versa. The need to troubleshoot BACnet communications

Resolution

Network captures are beneficial in troubleshooting the following cases:

  1. Connection issues between SmartStruxure client and AS/ES.
    • If customers complain their client cannot connect to an AS/ES, a capture run from the client PC can be very useful. However, SmartStruxure uses TCP/HTTP and the payload is not easy to decode. There are no Wireshark decoders to help out, but the good news is that there is in communication logging built in to SmartStruxure that can replace the need for network captures. (See Error logs from the Enterprise Server for ES and see Error logs from an Automation Server and Enterprise Server for AS)
  2. Communication Status problems between servers and controllers (for example BACnet controllers).
    • The location of where the captures is taken can be very important. The best place to capture is at a switch directly connected to the controller. This may be difficult because it will require putting a “dumb” hub between the switch and the controller or finding a port mirroring switch.
  3. When you are not receiving BACnet alarms when expected.
  4. When you are not receiving COV notifications when expected
  5. When a trendlog is trending external point
  6. To evaluate the health of a network.
  7. ARP broadcast traffic can flood networks and can create connectivity problems on BACnet/IP networks. If this is the case then a customer can take action by segmenting their BMS to a VLAN.
  8. Performance problems on graphics where a large number of the point displayed are BACnet
  9. MS/TP bus performance is poor or MS/TP device is offline
  10. Using a USB RS-485 adapter can permit the capture of packets on an MS/TP bus. Wireshark can then be used to decode the packet captures. This can show token passing problems as well as traffic loads.

Also check out the BACnet-Capturing MS/TP Traffic Quick-Help video on the Exchange.

Labels (1)
Labels:
  • EcoStruxure Building Operation
Tags (2)
  • Find more articles tagged with:
  • 14916
  • losing
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.