Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Schneider Electric Community
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
  • About Samart_Ploypradab
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Samart_Ploypradab
Samart_Ploypradab
Contributor
‎2026-06-28
37
Posts
1
Like Received
6
Likes Given
1
Solution

Community Badges

Open Hailing Frequencies - L3
Resistance is Futile - L3
Open Hailing Frequencies - L2
Resistance is Futile - L2
+7
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
Samart_Ploypradab
Samart_Ploypradab Contributor

Replacement model of the ION92830 (China)

Hi All Could you please find a replacement model of the ION92830 originally from China?
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1156 0 2

2024-01-16 08:45 PM

Samart_Ploypradab
Samart_Ploypradab Contributor

Configuring PM2200 for PT 600V/400V above Default Selection

How do I configure the PM2200/PM5000 when the customer is using PT (Potential Transformer) with a voltage rating of 600V/400V, which is higher than th...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
988 0 1

2023-11-08 06:33 AM

Samart_Ploypradab
Samart_Ploypradab Contributor

PAS800 Server Panel Historical Data Access

Does the PS800 Server Panel allow PME or 3rd party software to access its historical data? Via Protocol?It similar like PME able to read datalog in Po...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
6965 0 20

2023-09-25 03:10 PM

Samart_Ploypradab
Samart_Ploypradab Contributor

Can PM2000 or PM5000 meters be used in replacement of EM7200 meters?

Good day, everyone. Which meter type (PM2000 or PM5000) can be used to replace the EasyLogicTM EM7200 series Smart Demand Controller? Regards
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1557 0 2

2022-06-20 07:16 AM

Samart_Ploypradab
Samart_Ploypradab Contributor

Panal Server with Cloud connection

Hi All Kindly notify me when Cloud Connection Commissioning & Diagnostic (PAS600) will be available.Is that a Facility Expert (SB) connectivity is ope...
EcoStruxure Power & Grid icon_circle Gateways and Energy Servers
1684 0 3

2022-04-03 08:18 PM

Samart_Ploypradab
Samart_Ploypradab Contributor

PM8240 Show Blank screen with red/green blinking LED status after conn...

The PM8240 4pcs at one of pumping station, when we connect Power Meter via Ethernet LAN cable, the screen of PM8240 is showed blank screen. but when w...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
4410 0 7

2022-01-20 05:29 AM

Samart_Ploypradab
Samart_Ploypradab Contributor

How to local manual override of Digital/Analog output card without CPU

Dear Friend I got some question from my customer about in emergency case, The CPU card fail of dead.Can manual send command directly to DO/AO card vi...
Industrial Automation icon_circle Modicon PAC Forum
1559 0 1

2020-03-29 09:54 AM

Activity Feed
  • Posted Re: export csv file to SFTP Server with PAS 800 on Gateways and Energy Servers. ‎2024-04-03 02:21 AM
  • Got a Like for Re: Replacement model of the ION92830 (China). ‎2024-01-30 09:35 AM
  • Posted Re: Replacement model of the ION92830 (China) on Metering & Power Quality. ‎2024-01-29 09:40 PM
  • Posted Replacement model of the ION92830 (China) on Metering & Power Quality. ‎2024-01-16 08:45 PM
  • Tagged Replacement model of the ION92830 (China) on Metering & Power Quality. ‎2024-01-16 08:45 PM
  • Posted Configuring PM2200 for PT 600V/400V above Default Selection on Metering & Power Quality. ‎2023-11-08 06:33 AM
  • Tagged Configuring PM2200 for PT 600V/400V above Default Selection on Metering & Power Quality. ‎2023-11-08 06:33 AM
  • Posted Re: PAS800 Server Panel Historical Data Access on Gateways and Energy Servers. ‎2023-09-26 04:35 AM
  • Posted PAS800 Server Panel Historical Data Access on Gateways and Energy Servers. ‎2023-09-25 03:10 PM
  • Tagged PAS800 Server Panel Historical Data Access on Gateways and Energy Servers. ‎2023-09-25 03:10 PM
  • Liked Panel Server - wireless devices support for RPayumo. ‎2023-07-03 09:13 PM
  • Liked Panel Server video - Custom Model creation - EPC-Web for Szymon_Hochół. ‎2023-07-03 09:01 PM
  • Posted Re: SSL protocol error with EBX510 with google Chrome on Gateways and Energy Servers. ‎2022-06-20 07:38 AM
  • Tagged Re: SSL protocol error with EBX510 with google Chrome on Gateways and Energy Servers. ‎2022-06-20 07:38 AM
  • Posted Can PM2000 or PM5000 meters be used in replacement of EM7200 meters? on Metering & Power Quality. ‎2022-06-20 07:16 AM
  • Tagged Can PM2000 or PM5000 meters be used in replacement of EM7200 meters? on Metering & Power Quality. ‎2022-06-20 07:16 AM
  • Posted Re: EcoStruxure Panel Server: Our new Generation of Gateways on Gateways and Energy Servers. ‎2022-06-13 11:57 PM
  • Tagged Re: EcoStruxure Panel Server: Our new Generation of Gateways on Gateways and Energy Servers. ‎2022-06-13 11:57 PM
  • Liked Re: Panal Server with Cloud connection for Szymon_Hochół. ‎2022-04-15 01:31 AM
  • Posted Re: Panal Server with Cloud connection on Gateways and Energy Servers. ‎2022-04-04 02:17 AM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.