Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
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
  • About pawel_kowalski_
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
pawel_kowalski_
pawel_kowalski_
Commander
‎2025-12-14
256
Posts
53
Likes Received
44
Likes Given
3
Solutions

Community Badges

Open Hailing Frequencies - L6
Resistance is Futile - L6
Live Long and Prosper - L5
Open Hailing Frequencies - L5
+17
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
pawel_kowalski_
Commander pawel_kowalski_

PLC M2XX and HMI with BACnet

Hi,I have two questions:Is it possible to run the BACnet protocol on any of the 2XX series PLCs?If so, how can this be done?Do any of the HMI panels s...
Industrial Automation icon_circle HVAC and Pumping Forum
746 0 1

2025-03-23 12:34 PM

pawel_kowalski_
Commander pawel_kowalski_

Send Modbus variables from M241 using Modbus RTU(Serial1) to HMI GTU3

Hi.I have to connect the HMI panel to the M241 controller via Modbus RTU but I don't know exactly how to do it, somewhere I only came across this arti...
Industrial Automation icon_circle HVAC and Pumping Forum
1773 0 4

2025-02-02 02:42 AM

pawel_kowalski_
Commander pawel_kowalski_

Persistent variables and input value from HMI

Hi,I need advice on how to properly input value from HMI to variable to persistent variables.Now if I input value from HMI and shut down and up power,...
Industrial Automation icon_circle HVAC and Pumping Forum
1640 0 2

2023-06-26 12:41 AM

pawel_kowalski_
Commander pawel_kowalski_

Time synchronization between HMI XBTGT and TM251

Hi,I want to time synchronize between XBTGT6330 and TM251.To program TM251 I use MachineExpert v2.1 and for HMI I use VijeoDesigner v6.2.12.PLC commun...
Industrial Automation icon_circle Machine and Motion Control Forum
1597 0 3

2023-06-24 05:33 AM

pawel_kowalski_
Commander pawel_kowalski_

Check communication with Modbus Serial (RTU) Slave

Hi, As I wrote in the topic now I need some advice on how to check communication with modbus slave device.Configuration what I have is below in the pi...
Industrial Automation icon_circle HVAC and Pumping Forum
2167 0 1

2023-06-11 11:23 PM

pawel_kowalski_
Commander pawel_kowalski_

Check communication with Modbus TCP Slave

Hi, How I can get information about no communication with Modbus TCP slave (1)?I want that signal to add red crosses on HMI informing that the display...
Industrial Automation icon_circle HVAC and Pumping Forum
2394 0 2

2023-06-06 12:00 AM

pawel_kowalski_
Commander pawel_kowalski_

HMI XBTGT6330 Vijeo Designer 6.2 time on graph

Hi, 1. How to show data time on the graph in Vijeo Designer ?2. It is possible to show units of value on the graph?
Industrial Automation icon_circle HVAC and Pumping Forum
2511 0 5

2023-06-04 11:26 PM

pawel_kowalski_
Commander pawel_kowalski_

TM251MESE connect modbus RTU device and read registers

Hi, again 🙂Now I need advice/help on how to connect with modbus device and read registers.I use TM251MESE controller and I connect to them using a se...
Industrial Automation icon_circle Machine and Motion Control Forum
2472 0 3

2023-06-01 05:37 AM

pawel_kowalski_
Commander pawel_kowalski_

Show Real Value on HMI using Modbus TCP connection

Hi, I have a problem with how to show on HMI XBTGT4330 real value e.g. 123.553I read the water flow from the water meter as 32-bit register on PLC I h...
Industrial Automation icon_circle HVAC and Pumping Forum
3075 0 7

2023-05-26 01:30 AM

pawel_kowalski_
Commander pawel_kowalski_

Connection 2 PLC and 2 HMI in different locations

Hi I need advice on how to do a connection like that : The PLC is TM251MESE, HMI's is XBTGT4330 and XBTGT7340The buildings are about 200 meters apart,...
Industrial Automation icon_circle HVAC and Pumping Forum
918 0 0

2023-05-19 01:13 AM

pawel_kowalski_
Commander pawel_kowalski_

Connection 2 PLC and 2 HMI in different locations

Hi I need advice on how to do a connection like that :The PLC is TM251MESE, HMI's is XBTGT4330 and XBTGT7340The buildings are about 200 meters apart,...
Industrial Automation icon_circle EcoStruxure Automation Expert / IEC 61499 Forum
1352 0 1

2023-05-17 12:54 PM

Activity Feed
  • Liked Re: PLC M2XX and HMI with BACnet for Bastian_Schmitz. ‎2025-03-26 11:10 PM
  • Posted PLC M2XX and HMI with BACnet on HVAC and Pumping Forum. ‎2025-03-23 12:34 PM
  • Tagged PLC M2XX and HMI with BACnet on HVAC and Pumping Forum. ‎2025-03-23 12:34 PM
  • Posted Re: Send Modbus variables from M241 using Modbus RTU(Serial1) to HMI GTU3 on HVAC and Pumping Forum. ‎2025-02-11 12:33 AM
  • Posted Re: Send Modbus variables from M241 using Modbus RTU(Serial1) to HMI GTU3 on HVAC and Pumping Forum. ‎2025-02-09 04:15 AM
  • Liked Re: Send Modbus variables from M241 using Modbus RTU(Serial1) to HMI GTU3 for LeTomas. ‎2025-02-03 01:36 AM
  • Posted Send Modbus variables from M241 using Modbus RTU(Serial1) to HMI GTU3 on HVAC and Pumping Forum. ‎2025-02-02 02:42 AM
  • Tagged Send Modbus variables from M241 using Modbus RTU(Serial1) to HMI GTU3 on HVAC and Pumping Forum. ‎2025-02-02 02:42 AM
  • Posted Re: Time synchronization between HMI XBTGT and TM251 on Machine and Motion Control Forum. ‎2023-07-07 12:32 AM
  • Posted Re: Persistent variables and input value from HMI on HVAC and Pumping Forum. ‎2023-07-07 12:30 AM
  • Posted Re: Time synchronization between HMI XBTGT and TM251 on Machine and Motion Control Forum. ‎2023-06-28 01:22 PM
  • Posted Persistent variables and input value from HMI on HVAC and Pumping Forum. ‎2023-06-26 12:41 AM
  • Tagged Persistent variables and input value from HMI on HVAC and Pumping Forum. ‎2023-06-26 12:41 AM
  • Posted Time synchronization between HMI XBTGT and TM251 on Machine and Motion Control Forum. ‎2023-06-24 05:33 AM
  • Tagged Time synchronization between HMI XBTGT and TM251 on Machine and Motion Control Forum. ‎2023-06-24 05:33 AM
  • Posted Re: HMI XBTGT6330 Vijeo Designer 6.2 time on graph on HVAC and Pumping Forum. ‎2023-06-12 12:08 AM
  • Posted Check communication with Modbus Serial (RTU) Slave on HVAC and Pumping Forum. ‎2023-06-11 11:23 PM
  • Tagged Check communication with Modbus Serial (RTU) Slave on HVAC and Pumping Forum. ‎2023-06-11 11:23 PM
  • Posted Re: Check communication with Modbus TCP Slave on HVAC and Pumping Forum. ‎2023-06-08 11:51 AM
  • Posted Check communication with Modbus TCP Slave on HVAC and Pumping Forum. ‎2023-06-06 12:00 AM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.