Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
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
  • About dnordenberg1
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
dnordenberg1
dnordenberg1
Lt. Commander
‎2025-11-23
103
Posts
47
Likes Received
36
Likes Given
0
Solutions

Community Badges

Open Hailing Frequencies - L5
Live Long and Prosper - L4
Open Hailing Frequencies - L4
Live Long and Prosper - L3
+10
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
dnordenberg1
Lt. Commander dnordenberg1

ESME M251 BOOL variable in OPC UA and modbus simultaneously

Hi! TLDR;How can I have an BOOL variable that is read/write in both modbus TCP server and from OPC UA at the same time? Since the OPCUASymbolConfigura...
Industrial Automation icon_circle Machine and Motion Control Forum
282 0 0

2025-07-09 09:21 AM

dnordenberg1
Lt. Commander dnordenberg1

Machine Expert exporting %QX signals to OPC UA symbols.

Hi!Machine Expert is hiding these in the symbol configuration. I found the option for it in pure codesys Object: Symbol Configuration called direct I/...
Industrial Automation icon_circle Machine and Motion Control Forum
379 0 0

2025-04-17 06:09 AM

dnordenberg1
Lt. Commander dnordenberg1

Aveva System Platform with M340/M580 (EcoStruxure™ Modicon Communicati...

Hi!We have quite a few modicon controllers and are migrating from a very old third party SCADA to ASP.We hired a consulting firm that is great at ASP ...
Industrial Automation icon_circle Industry Automation and Control Forum
1669 1 6

2025-04-17 05:42 AM

dnordenberg1
Lt. Commander dnordenberg1

Control Expert 16.1 gone?

Hi!Where did Control Expert 16.1 go? Is there something we should know about regarding using it? Kind regardsDavid
Industrial Automation icon_circle Modicon PAC Forum
3463 0 6

2025-04-07 07:50 AM

dnordenberg1
Lt. Commander dnordenberg1

Show/hide pins on DFBs to be able to create more generic/dynamic DFBs ...

Unlike many other PLC programming software, Control Expert does not allow you to create your own dynamically sized blocks. For example in Codesys/Mach...
Industrial Automation icon_circle Modicon Ideas & new features
583 6 2

2025-01-31 01:18 AM

dnordenberg1
Lt. Commander dnordenberg1

Control Expert Variable selection enhancements

Hi!Please make variable selection from code segments easier with "find as you type" like behaviour like (more like Machine Expert). You can start typi...
Industrial Automation icon_circle Modicon Ideas & new features
352 4 0

2025-01-31 12:02 AM

dnordenberg1
Lt. Commander dnordenberg1

Wishlist Dark theme uniform experience in Control Expert

Hi!Can we please have a dark mode in EcoStruxure Control Expert? I know colors can be edited but there are so many things that you can't change so it ...
Industrial Automation icon_circle Modicon PAC Forum
586 5 2

2025-01-24 06:18 AM

dnordenberg1
Lt. Commander dnordenberg1

M580 DTM Modbus request bits, where are they?

In device DDT we have DIO control and health bits which are called 513-640 and it say 1 BIT per DIO. These numbers corresponds nicely with the number...
Industrial Automation icon_circle Industry Automation and Control Forum
619 0 0

2024-07-31 02:54 AM

dnordenberg1
Lt. Commander dnordenberg1

Ways to use EBOOL (%M) in DDT

Hi!I guess everyone knows about the short coming that EBOOL can't be used in a DDT (https://community.se.com/t5/Modicon-PAC-Forum/EBOOL-in-DDT/m-p/460...
Industrial Automation icon_circle Modicon PAC Forum
2196 0 1

2024-07-08 12:18 AM

dnordenberg1
Lt. Commander dnordenberg1

Using read_var and write_var trigged in series

HiFor the real question, jump straight to TL;DR. But here comes some background story first...I have a "modbus TCP" slave that refuse to handle more t...
Industrial Automation icon_circle Modicon PAC Forum
8066 1 7

2024-05-20 12:21 PM

dnordenberg1
Lt. Commander dnordenberg1

Editable named/structured variable names for generic modbus DTM IO sca...

Hi!Since the DTM browser does not allow any change inside a modbus device request without a offline build I tried to find a nicer way around that and ...
Industrial Automation icon_circle Modicon PAC Forum
1416 0 2

2024-02-05 09:53 AM

Activity Feed
  • Posted Re: Can you use += in Machine Expert like you can Java and C++ etc? on Industry Automation and Control Forum. ‎2025-11-19 09:46 PM
  • Liked Re: Aveva System Platform with M340/M580 (EcoStruxure™ Modicon Communication Server vs EcoStruxure™ OPC UA Server Expert) for Sumanjith.an. ‎2025-11-01 01:18 PM
  • Liked Re: Modicon M580 dPAC Immunity to Radio Frequency for YONGHO-KIM. ‎2025-11-01 01:06 PM
  • Got a Like for Aveva System Platform with M340/M580 (EcoStruxure™ Modicon Communication Server vs EcoStruxure™ OPC UA Server Expert). ‎2025-10-27 05:25 AM
  • Liked Re: What is the project setting "Data memory protect" for? for Trinxs1. ‎2025-10-01 07:40 AM
  • Liked Control Expert: Support for Single-Line Comments (//) in ST Editor for Snacky. ‎2025-10-01 07:39 AM
  • Liked Re: CE 16.2 Ethernet IP Devices. for ciupol. ‎2025-10-01 07:26 AM
  • Got a Like for Control Expert Variable selection enhancements. ‎2025-10-01 03:02 AM
  • Got a Like for M580 DTM browser - allow changes online. ‎2025-10-01 03:01 AM
  • Posted Re: DTM Audit Tool on Modicon PAC Forum. ‎2025-09-27 08:43 AM
  • Posted Re: CE 16.2 Ethernet IP Devices. on Modicon PAC Forum. ‎2025-09-27 07:28 AM
  • Posted Re: Freshness on Industry Automation and Control Forum. ‎2025-09-25 10:20 PM
  • Got a Like for Re: DTM Audit Tool. ‎2025-09-24 01:33 AM
  • Posted Re: DTM Audit Tool on Modicon PAC Forum. ‎2025-09-20 01:54 PM
  • Got a Like for Show/hide pins on DFBs to be able to create more generic/dynamic DFBs without loads of unused pins displaying in the code. ‎2025-08-12 12:18 AM
  • Got a Like for Show/hide pins on DFBs to be able to create more generic/dynamic DFBs without loads of unused pins displaying in the code. ‎2025-07-23 02:00 AM
  • Got a Like for Re: EcoStructure Machine Expert V2.2. ‎2025-07-19 09:38 PM
  • Posted Re: EcoStructure Machine Expert V2.2 on Machine and Motion Control Forum. ‎2025-07-19 07:35 AM
  • Got a Like for Show/hide pins on DFBs to be able to create more generic/dynamic DFBs without loads of unused pins displaying in the code. ‎2025-07-09 09:44 PM
  • Posted ESME M251 BOOL variable in OPC UA and modbus simultaneously on Machine and Motion Control Forum. ‎2025-07-09 09:21 AM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.