Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

ESME M251 BOOL variable in OPC UA and modbus simultaneously

Machine and Motion Control Forum

Support forum for Machine and Motion Control solutions, including Lexium MC12 and robotics, PacDrive, Modicon PLCs and I/Os, EcoStruxure Machine Expert Twin, … - from design, implementation to troubleshooting and more, by Schneider Electric
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
  • Industrial Automation
  • Machine and Motion Control Forum
  • ESME M251 BOOL variable in OPC UA and modbus simultaneously
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Bastian_Schmitz
Admiral Bastian_Schmitz Admiral
9
FernandoRodrigues
FernandoRodrigues Support
7
LeTomas
Lt. Commander LeTomas Lt. Commander
5
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Alliance Partner Program System Integrator

Related Products
product field
Schneider Electric
EcoStruxure™ Machine Expert
product field
Schneider Electric
Logic Controller - Modicon M251

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Machine and Motion Control Forum
Start a Topic
dnordenberg1
Lt. Commander dnordenberg1
Lt. Commander

Posted: ‎2025-07-09 09:21 AM . Last Modified: ‎2025-07-10 07:11 AM

0 Likes
0
281
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
Posted: ‎2025-07-09 09:21 AM . Last Modified: ‎2025-07-10 07:11 AM

ESME M251 BOOL variable in OPC UA and modbus simultaneously

Hi!

 

TLDR;

How can I have an BOOL variable that is read/write in both modbus TCP server and from OPC UA at the same time?

 

Since the OPCUASymbolConfiguration forbids %QX addressed variables being in the list I can not use the build in modbus TCP server which uses %QX for modbus coils. I switched to using FB_ModbusTcpServer instead only to discover it can't use port 502 even when built in modbus TCP server is removed from the interface 😞

But anyway I changed my BOOLs to %MX.n addressing and added my array of BOOLs to the FBs coils pin and went back to the OPCUASymbolConfiguration only to discover that variables that has an %MX address is not allowed either 😞

So how should I do it then? It seems like an impossible combination. Since I want read/write access from both ways I can't just simply make a second variable and assign it the value of another since it would be a one way assignment. I also tried using VAR_CONFIG which then makes the address syntax %Q* or %M* in my main variable list and that fools OPCUASymbolConfiguration to allow it and then I add the complete %MX.n address of it in the VAR_CONFIG list. This semi works, I can toggle the BOOL from modbus but the OPC UA symbol seems to be read only. It displays symbol status but nothing happens when I toogle it 😞

 

Kind regards

David

Labels
  • Labels:
  • Programming and Software Development
  • Technical Support and Troubleshooting
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.