intermittent fault won't reset on XTU300
Dear
We have an intermittent fault via communication on the XTU300, but when looking at the XML the fault isn't there any more.
The fault has been resetted.
Even with a communication reset it won't go a way. (I have send FFFF to register 10)
Does someone have other suggestions?
Thanks in advance
Jeroen
- Labels:
-
Insulation Monitoring
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
I believe we solved this question via email-
If someone has similar issue, specifically when there are a lot of vigilohm XML, XL, XD308c connected to the interface, please get in touch with me.
Symptom is that there are intermittent communication losses between the interface and its slaves. Communication is restored when the interface is power cycled.
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
Hello
It's not the seem we discussed via mail. This one doesn't lose its measurements.
But I can put logging on the communication of the bus to check if they occur on the same time.
regards
Jeroen