Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84796members
354244posts

intermittent fault won't reset on XTU300

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

JeroenDeville
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
2
554

intermittent fault won't reset on XTU300

Dear

 

We have an intermittent fault via communication on the XTU300, but when looking at the XML the fault isn't there any more.

The fault has been resetted.

Even with a communication reset it won't go a way. (I have send FFFF to register 10)

 

Does someone have other suggestions?

Thanks in advance

 

Jeroen

2 Replies 2
Madleen_Laclef
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
1
539

Re: intermittent fault won't reset on XTU300

I believe we solved this question via email-

If someone has similar issue, specifically when there are a lot of vigilohm XML, XL, XD308c connected to the interface, please get in touch with me.

Symptom is that there are intermittent communication losses between the interface and its slaves. Communication is restored when the interface is power cycled.

JeroenDeville
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
539

Re: intermittent fault won't reset on XTU300

Hello

It's not the seem we discussed via mail. This one doesn't lose its measurements.

But I can put  logging on the communication  of the bus to check if they occur on the same time.

regards

Jeroen