Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84584members
353853posts

What includes the BCPMSCA60S reference

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
YvesR
Ensign Ensign
Ensign
0 Likes
1
243

What includes the BCPMSCA60S reference

Hello,

I want to quote a BCPM split core

when order the BCPMSCA60S reference is included;

main unit

board for CT connection

cable between main unit and board (round or flat)

and 60 50A CT's?

Thanks in advance?

Yves


Accepted Solutions
Adam_Hardman
Commander Commander
Commander
0 Likes
0
224

Re: What includes the BCPMSCA60S reference

Models with more than 2 as the number of circuits include 50 A branch CTs with 2 meter leads and 1.8M round ribbon cables.

The BCPMSC models with 1, 2 or Y63 as the number of circuits DO NOT INCLUDE ANY branch CTs or ribbon cables (they include only the Main board and adapater board assemblies) . These models are provided to allow users to order a

specific combination of CT quantities, CT sizes, CT lead lengths and ribbon cable styles and lengths.

The CTs and cables must be ordered separately.

The PowerLogic BCPMSC uses .333 V AC output split-core CTs for the auxiliary inputs. These CTs are ordered separately from the BCPM.

See Answer In Context

1 Reply 1
Adam_Hardman
Commander Commander
Commander
0 Likes
0
225

Re: What includes the BCPMSCA60S reference

Models with more than 2 as the number of circuits include 50 A branch CTs with 2 meter leads and 1.8M round ribbon cables.

The BCPMSC models with 1, 2 or Y63 as the number of circuits DO NOT INCLUDE ANY branch CTs or ribbon cables (they include only the Main board and adapater board assemblies) . These models are provided to allow users to order a

specific combination of CT quantities, CT sizes, CT lead lengths and ribbon cable styles and lengths.

The CTs and cables must be ordered separately.

The PowerLogic BCPMSC uses .333 V AC output split-core CTs for the auxiliary inputs. These CTs are ordered separately from the BCPM.