Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84525members
353768posts

Vigilohm is now Safety Integrity Level 2 certified

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
Madleen_Laclef
Lt. Commander Lt. Commander
Lt. Commander

Vigilohm is now Safety Integrity Level 2 certified

The IM400 and IFL12MC series have received SIL 2 certification from a 3rd party official bureau. This demonstrates their high reliability and is a true differentiator from competitors: our offers keep monitoring the installation even in case of product internal fault.  

 

Access certificates here.

 

 

Tags (1)

Accepted Solutions
Nedjma
Community Alumni (Retired)
Community Alumni (Retired)
0 Likes
0
562

Re: Vigilohm is now Safety Integrity Level 2 certified

Hello @Madleen_Laclef,

 

Thanks for sharing this useful information with the community. 🙂

 

 

 

See Answer In Context

Tags (1)
1 Reply 1
Nedjma
Community Alumni (Retired)
Community Alumni (Retired)
0 Likes
0
563

Re: Vigilohm is now Safety Integrity Level 2 certified

Hello @Madleen_Laclef,

 

Thanks for sharing this useful information with the community. 🙂

 

 

 

Tags (1)