Hi Community,
I'm about to buy a new power meter M8650, and I've just receive a quotation wit this Order Number:
M8650-A0-C0-H6-E1-B-0-A-A633
However, at the datasheet "PowerLogic™ ION8650 series Technical Datasheet" just indicates 11 numbers so the "A633" number is not clear to me what means. I would really appreciate if someone could tell me what A633 means for ordering this meter.
Kind regards
Javier
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
Hello Javier,
The ION8650 meters have the ability to have custom order options. These are are usually referred to as AA codes. The AA codes could include specific firmware versions, specific template loaded at the factory or other custom features. Usually there is a specific reason why a custom order code is used.
Regards,
Charles
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
Hello Javier,
The ION8650 meters have the ability to have custom order options. These are are usually referred to as AA codes. The AA codes could include specific firmware versions, specific template loaded at the factory or other custom features. Usually there is a specific reason why a custom order code is used.
Regards,
Charles