Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Synchronizing ION 92040 via IRIG-B

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Synchronizing ION 92040 via IRIG-B
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
Ramasamy_N
Ramasamy_N Champion
117
View All

Recommended Forums

  • SmartConnector Forum

Related Products
product field
Schneider Electric
PowerLogic ION9000
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
ManuelTrebilcock
ManuelTrebilcock Contributor
Contributor

Posted: ‎2021-10-21 09:10 AM

0 Likes
2
3214
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
‎2021-10-21 09:10 AM

Synchronizing ION 92040 via IRIG-B

Hello everyone,

 

We are in the design phase of an architecture intended to synchronize 6 ION 92040 via IRIG-B. The time server must be a GE RT430.

In the ION manual is stated that you can connect an IRIG-B source to one of the meter's digital input for IRIG-B synchronization and that you must configure both, the meter's digital input and the meter's clock. I have the following questions: 

  • What's the configuration you have to do?
  • Which technique can be used to transmit the unmodulated code, TTL, RS232, RS485, etc, and how to connect it to the digital input properly?
  • Can you implement a daisy chain connection for the synchronization of all the meters?

 

Beforehand, thank you for your time.

 

 

Best regards,

 

Manuel Trebilcock

  • Thumbnail of PowerLogic ION9000
    Schneider Electric
    PowerLogic ION9000
View products (1)
Labels
  • Labels:
  • ION9000
Tags (3)
  • Tags:
  • english
  • ion9000
  • IRIG-B
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Yut
Yut
Leader

Posted: ‎2021-11-06 04:58 PM

0 Likes
0
3145
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
‎2021-11-06 04:58 PM

I'm working with the GPS Synchronize for long time. ION meter can do time synchronize as follow.

To serial port, the clock transmits signal in ASCII format such as Truetime/Datum meters can be daisy chain connected via RS-485 fashion network .

To IRIG-B port (On board DI), clock transmits signal in TTL, DCLS whatever the manufacturer of the clock called unmodulated type this can be daisy chain as long as the the total impedance do exceed the clock output capability i.e. 10k ohms in case of the Arbiter brand.

 

For service

If ASCII type, a computer install with Hyper Terminal software or any is needed for monitor the signal.

IF IRIG-B type, an oscilloscope is needed for monitor the signal.

 

Time sync. check can be done using diagnostics module output monitor see ION Reference. 

See Answer In Context

Tags (1)
  • Tags:
  • english
Reply
Replies 2
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2021-10-21 04:57 PM

1 Like
1
3206
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
‎2021-10-21 04:57 PM

Hello @ManuelTrebilcock 

 

For the configurations, there are 2 modules I know of that need to be configured. The clock module's time synchronization source and Digital input's mode needs to be set to IRIG-B

 

 

@DanL 

Do you know the answers to the questions:

  • Which technique can be used to transmit the unmodulated code, TTL, RS232, RS485, etc, and how to connect it to the digital input properly?
  • Can you implement a daisy chain connection for the synchronization of all the meters?

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Tags (1)
  • Tags:
  • english
Reply
Yut
Yut
Leader

Posted: ‎2021-11-06 04:58 PM

0 Likes
0
3145
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
‎2021-11-06 04:58 PM

I'm working with the GPS Synchronize for long time. ION meter can do time synchronize as follow.

To serial port, the clock transmits signal in ASCII format such as Truetime/Datum meters can be daisy chain connected via RS-485 fashion network .

To IRIG-B port (On board DI), clock transmits signal in TTL, DCLS whatever the manufacturer of the clock called unmodulated type this can be daisy chain as long as the the total impedance do exceed the clock output capability i.e. 10k ohms in case of the Arbiter brand.

 

For service

If ASCII type, a computer install with Hyper Terminal software or any is needed for monitor the signal.

IF IRIG-B type, an oscilloscope is needed for monitor the signal.

 

Time sync. check can be done using diagnostics module output monitor see ION Reference. 

Tags (1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.