Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Regarding meter side during withstand voltage test

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Regarding meter side during withstand voltage test
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Miyai
Miyai
Contributor

Posted: ‎2025-10-29 10:12 PM

0 Likes
3
682
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
‎2025-10-29 10:12 PM

Regarding meter side during withstand voltage test

Hello,


I'd like some advice on what to do when testing meter.

 

When performing a withstand voltage test or insulation resistance test after installing an ION9000, PM8000, or PM5000 on a panel, how do you handle voltage measurement circuit and control power supply circuit?

 

Also, how does the ION9000 handle ground wiring?
Do I need to disconnect ground wire from terminal?


Generally, if it is not possible to perform a withstand voltage test or the like, there will be a note in the manual.
However, I was unable to find any mention of this in the manual for the meter mentioned above.

 

Therefore, I would like some advice on wiring connections during testing.

 

Best regards,

Miyai

Labels
  • Labels:
  • ION9000
  • PM5000
  • PM8000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-10-30 08:30 AM

0 Likes
0
667
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
‎2025-10-30 08:30 AM

Hi @Miyai 

 

All ION meters are subjected to hi-pot testing during the manufacturing process, ensuring their dielectric integrity before deployment. As a result, repeating such tests in the field is not only unnecessary but can be harmful.

 

After factory testing, additional surge protection circuitry, typically consisting of MOVs, fuses, etc., is integrated into the meter to shield it from transient over voltages caused by lightning or upstream electrical disturbances.

 

While this protection enhances the meter’s resilience to real-world surge events, it also makes the meter vulnerable to damage if subjected to dielectric withstand voltage tests without first disconnecting these circuits and components. Therefore, performing hi-pot tests in the field without isolating the surge protection circuitry can inadvertently trigger or destroy these components, leading to meter failure.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

See Answer In Context

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-10-30 02:15 PM

0 Likes
1
653
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
‎2025-10-30 02:15 PM

Hello @Miyai ,

 

While the ION9000 and PM8000 meters do not mention Hi-pot specific, there is a comment under Safety precautions. "Do not exceed the maximum ratings of this device."  safety-precautions 

As Mehran has said the meter has protection devices that will save internal electronics however will cause the meter to no longer be operable.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 3
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-10-30 08:30 AM

0 Likes
0
668
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
‎2025-10-30 08:30 AM

Hi @Miyai 

 

All ION meters are subjected to hi-pot testing during the manufacturing process, ensuring their dielectric integrity before deployment. As a result, repeating such tests in the field is not only unnecessary but can be harmful.

 

After factory testing, additional surge protection circuitry, typically consisting of MOVs, fuses, etc., is integrated into the meter to shield it from transient over voltages caused by lightning or upstream electrical disturbances.

 

While this protection enhances the meter’s resilience to real-world surge events, it also makes the meter vulnerable to damage if subjected to dielectric withstand voltage tests without first disconnecting these circuits and components. Therefore, performing hi-pot tests in the field without isolating the surge protection circuitry can inadvertently trigger or destroy these components, leading to meter failure.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-10-30 02:15 PM

0 Likes
1
654
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
‎2025-10-30 02:15 PM

Hello @Miyai ,

 

While the ION9000 and PM8000 meters do not mention Hi-pot specific, there is a comment under Safety precautions. "Do not exceed the maximum ratings of this device."  safety-precautions 

As Mehran has said the meter has protection devices that will save internal electronics however will cause the meter to no longer be operable.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
Miyai
Miyai
Contributor

Posted: ‎2025-11-04 09:00 PM

0 Likes
0
609
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
‎2025-11-04 09:00 PM

Hello @Charles_Murison , @Mehran_Mehrnia 

 

Thank you for advice.
I will exclude the meter from the voltage withstand test.

 

 

Best regards,

Miyai
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.