Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Modbus Baud rate iEM2050/iEM2055 series single phase energy meter

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Modbus Baud rate iEM2050/iEM2055 series single phase energy meter
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
AndersDahlskog
AndersDahlskog Contributor
Contributor

Posted: ‎2025-10-25 12:58 AM

0 Likes
1
1947
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
‎2025-10-25 12:58 AM

Modbus Baud rate iEM2050/iEM2055 series single phase energy meter

Hi

According to User Manual PHA6516400-05 page 16 it states that the baud rate can be set to higher value than 9600 (38400/19200).

If so really good then using this meter together with other =S= meters and Panel Server that has baud rate 19200 as standard setting.

Baud rate 9600 is stated in earlier versions of the User Manual and also in the hardware was this the highest baud rate possible to set.

Has there been an hardware upgrade and if so from what date code ?

Wrong in User Manual ?

 

BR/Anders

PAE EcoStruxure Power, Sweden

Labels
  • Labels:
  • iEM2000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Jesus_Diaz
Jesus_Diaz Leader
Leader

Posted: ‎2025-11-04 10:06 AM

1 Like
0
1819
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
‎2025-11-04 10:06 AM

Hi @AndersDahlskog,

 

I'm sorry for the delay; I was gathering the information.


There were some hardware changes in the iEM2050 and iEM2055 to support higher baud rates. For the iEM2050, the start date is 17 June 2024, and for the iEM2055, it is 29 July 2024.

 

Best Regards,

JD

See Answer In Context

Reply
Reply 1
Jesus_Diaz
Jesus_Diaz Leader
Leader

Posted: ‎2025-11-04 10:06 AM

1 Like
0
1819
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
‎2025-11-04 10:06 AM

Hi @AndersDahlskog,

 

I'm sorry for the delay; I was gathering the information.


There were some hardware changes in the iEM2050 and iEM2055 to support higher baud rates. For the iEM2050, the start date is 17 June 2024, and for the iEM2055, it is 29 July 2024.

 

Best Regards,

JD
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.