Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84468members
353683posts

Phasor diagram in PM5560 vs ION

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
engineer_langfo
Lieutenant JG
Lieutenant JG
0 Likes
1
423

Phasor diagram in PM5560 vs ION

Hello -  I have noticed an inconsistency between the phasor diagram is represented in the PM5560 and the convention used in ION series meters.

The screen capture from page 136 of the PM5560 manual shows a ACB rotation; but nowhere is it indicated as such. 

Whereas; the ION7550 manual screen capture is more detailed identifying the ABC rotation.

Can someone please confirm the convention used in the PM5560?    Since ACB is a standard rotation for most wiring.

Any idea why this may appear to be different ?? 

Or could someone please add some clarification. 

Thanks!

5762

5763


Accepted Solutions
Cesar_Torralba
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: Phasor diagram in PM5560 vs ION

Hi Eric,

The factory default setting for all PM5500 series meters is ABC rotation.  The diagram you are referring to comes from the PF chapter, and is only shown there as an example.  The intent of that diagram is not to show phase rotation, but rather to show how current leads or lags the voltage waveform, depending on the type of load (capacitive or inductive).  That is why I showed only one V and I phase on the linear axis.  If you want to see how phasors work in the PM5560, please refer to Chapter 4, page 125.

5764

Hope this helps.

Cesar

See Answer In Context

1 Reply 1
Cesar_Torralba
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: Phasor diagram in PM5560 vs ION

Hi Eric,

The factory default setting for all PM5500 series meters is ABC rotation.  The diagram you are referring to comes from the PF chapter, and is only shown there as an example.  The intent of that diagram is not to show phase rotation, but rather to show how current leads or lags the voltage waveform, depending on the type of load (capacitive or inductive).  That is why I showed only one V and I phase on the linear axis.  If you want to see how phasors work in the PM5560, please refer to Chapter 4, page 125.

5764

Hope this helps.

Cesar