Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
Hi,
Working on a request from customer to obtain information pertaining to below via MODBUS.
It seems, address 30222 reflect 3-phase data instead of phase A.
Whereas for address 30236 and 30250, no valid data available.
This is observed both in PM8240 and ION9000.
Firmware upgraded to latest.
Also tried various voltage mode.
Active Power Del A Last Demand [ Modbus 30222 ]
Active Power Del B Last Demand [ Modbus 30236 ]
Active Power Del C Last Demand [ Modbus 30250 ]
Would expect above very much collated to Active Power A,B,C.
But instead, the observation is 30222 reflect total of 3054 + 3056 + 3058
Active Power A [ Modbus 3054 ]
Active Power B [ Modbus 3056 ]
Active Power C [ Modbus 3058 ]
Any advice?
Link copied. Please paste this link to share this article on your social media post.
Hello @TC ,
30222 , 30236 and 30250 these measurements are not per phase values but Rates A, Rate B, Rate C and Rate D (30264).
The default Modbus register list does not have the measurement you are looking for. With the power of ION, it is possible to make a custom framework that is able to get the information you are looking for and link to new Modbus registers.
You would need to make 3 sliding windows demand modules (SWD), linking the per phase kw readings from the power meter module. The output of the SWD module can be linked to new Modbus Slave Modules.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hello @TC ,
You could look into using something like a store module that only updates the outputs when the store input is pulsed. For the minx, max, and average, you will likely want to use a feedback module to pulse the reset input once the value is saved, either in data recorder, store module or both.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hello @TC ,
30222 , 30236 and 30250 these measurements are not per phase values but Rates A, Rate B, Rate C and Rate D (30264).
The default Modbus register list does not have the measurement you are looking for. With the power of ION, it is possible to make a custom framework that is able to get the information you are looking for and link to new Modbus registers.
You would need to make 3 sliding windows demand modules (SWD), linking the per phase kw readings from the power meter module. The output of the SWD module can be linked to new Modbus Slave Modules.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Hi all, working on the full expectation of customer and hoping to get some advice:
The requirement is "At the end of demand interval, to report the min, max, average of each phase. kW and kVA".
What is the most optimized way to achieve this?
Currently exploring with min, max, and ave module which is not exactly matching the expectation.
Struggling with the need to add "processing" so that the values are reported only once at end of demand interval, before resetting.
Hope to get some guidance. Thank you!
(I have attached PPT, and video for better grasp of my situation)
Link copied. Please paste this link to share this article on your social media post.
Hello @TC ,
You could look into using something like a store module that only updates the outputs when the store input is pulsed. For the minx, max, and average, you will likely want to use a feedback module to pulse the reset input once the value is saved, either in data recorder, store module or both.
Regards,
Charles
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.