Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Hello @BlueHen ,
The PME driver for PM5563 will collect the Energy values from the onboard logs of the meter. If the logging has stopped there are 2 common possibilities.
a) Logging on the device itself has stopped
b) PME driver has changed to use basic modbus driver (does not including onboard logs) from default driver (one specific to the PM5000 series).
Option a) could use third party tools such as ION Setup to check, possibly modbus commands to confirm logging is increasing.
Option b) Often this happens when someone uses the Device Type editor to add additional loging to the device and uses the Install device option that in some versions of PME would also change the device driver to use generic modbus device, effectively turning of onboard log collection. Recommend working with your local technical support to confirm if this did happen and steps to correct. Suggest collecting diagnostic tool output in PME when contacting technical support.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hello @BlueHen ,
The PME driver for PM5563 will collect the Energy values from the onboard logs of the meter. If the logging has stopped there are 2 common possibilities.
a) Logging on the device itself has stopped
b) PME driver has changed to use basic modbus driver (does not including onboard logs) from default driver (one specific to the PM5000 series).
Option a) could use third party tools such as ION Setup to check, possibly modbus commands to confirm logging is increasing.
Option b) Often this happens when someone uses the Device Type editor to add additional loging to the device and uses the Install device option that in some versions of PME would also change the device driver to use generic modbus device, effectively turning of onboard log collection. Recommend working with your local technical support to confirm if this did happen and steps to correct. Suggest collecting diagnostic tool output in PME when contacting technical support.
Regards,
Charles
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.